Part Number: TLV9354-Q1 Hi there,
About bypass capacitor capacity between V+ and V- terminals,
The datasheet seems to recommend a capacitor value of 0.1uF.
Is there any problem when setting the capacitance of this capacitor to 1uF?
Best…
Part Number: TLV9354-Q1 Other Parts Discussed in Thread: TLV9154-Q1 Hi team,
Could you please give me the "Voltage output swing from rail" value over operating temp range of TLV9354-Q1 and TLVx197-Q1
just as specified in TLV915x-Q1 datasheet?
…
Other Parts Discussed in Thread: TLV4197-Q1 , OPA4197-Q1 , TLV9354-Q1 Hello Team,
I am looking for amplifier with below specifications: Input voltage > 4.5V
Output voltage > 5V
Slew rate - 20 V/uS
Package - 14 - pin TSSOP (Quad channel)
Automotive…
Hi Nuno,
I have found these here:
https://www.ti.com/assets/js/compareParts/compare.html?familyId=1293&parts=OPA4196,OPA4191,OPA4171-Q1,OPA4171,TLV4171,OPA4130,TLV9154-Q1,OPA4991-Q1,TLV9154,OPA4991,TLV9354-Q1,TLV9354,TLV2444,TLV2444A,LMP7704&cols…
Frank,
First off, TLV9304QPWRQ1 is NOT an op amp but comparator so you may not use it in your application.
When it comes to LM2902B-Q1 (SR of 0.5V/us) vs TLV9354QPWRQ1 (20V/us), you may not see much difference in the output rate of change because…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…