Part Number: TLV9364 Other Parts Discussed in Thread: TLV9164 , Hello.
While reviewing the datasheet, I'm writing to inquire about the correct dimensions for the TSSOP(14) package: the dimensions on the first page or the dimensions in the PACKAGE OUTLINE…
Part Number: TLV9364 Hello,
Is there an open loop gain and phase plot available to review for the TLV9364? I do not see one on the datasheet.
Thank you,
Nick
Hi Abhishek,
There are a number of ADC devices that have an integrated PGAs that can be used in the signal chain with the PGA848.
For example, the middle pin A1 can be hard wired to be 0, resulting in gains of 0.5, 1, 10, and 20 from the PGA848. The…
Part Number: TLV9034-Q1 Other Parts Discussed in Thread: LM2902B , LM2902B-Q1 , LM2902 , TLV9354 , TLV9364-Q1 , TLV9364 Tool/software: Hi Team,
We were using LM2902B-Q1 before for a current sense op amp. While the slew rate of the LM2902B is slow, then…
Part Number: NE5534A Other Parts Discussed in Thread: TLV9364 Hello,
We are seeing NE5534AD are Last buy process now and it is going to EOL announced by PDN# 20230522005.3
This OP-amp was employed on many of Audio application with a unique sound characteristics…
Part Number: OPA4991 Other Parts Discussed in Thread: TLV9364 , OPA4992 Tool/software: Hi,
One of my customers recently reached out to me with an issue where the slew rate they are seeing from the device is off by an order of magnitude than what they…
Part Number: LM224A Other Parts Discussed in Thread: TLV9354 , TLV9364 , TLV9054 , TLV9064 Hi team,
Do we have p2p solution with better bandwidth to replace LM224ADR?
BR,
Jimmy
Part Number: TLV9354 Other Parts Discussed in Thread: TLV9364 , OPA1679 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I was thinking of using the TLV9354 part in a circuit where low sensitivity to temperature in regards…
Hey Kevin,
OPA4992 seems to be the best competitor to MC33079. Here is a comparison table. If cost is a concern, consider TLV9364, or if 30V supply is not needed, they could also cost-down to TLV9164.
► Part Number
OPA4992
MC33079
…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…