Part Number: TMDSCNCD28388D Other Parts Discussed in Thread: C2000WARE
HI
Want to realize that under the enet_lwip routine, the development board is connected to the switch through a network cable, so that the development board automatically obtains…
Is there anyone here?
https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1012170/tmdscncd28388d-can-fd-rx-interrupt?tisearch=e2e-sitesearch&keymatch=can-fd
I've seen several Q&A including…
Part Number: TMS320F28388D Other Parts Discussed in Thread: DP83822I , C2000WARE , TMDSCNCD28388D Hi,
I want to implement Ethernet loopback between Laptop and TMS320F28388D. I would like to know how to start to realize this. The board is ready, and…
Hi Carlos,
I assume your question was regarding the electrical trace, if it looses the contact to BGA package than you are trying to fix it?
BGA hardware design rules to be followed based on specific pitch.
Please refer to C2000 Control card example…
Do you take a look at the application reports as the below links which can be found in the folder of "C:\ti\c2000\C2000Ware_MotorControl_SDK_4_00_00_00\solutions\tmdxiddk379d\docs". Please note that the examples is based on the TI EVM kits ( TMDXIDDK379D…
I have only one board. A experimenter kit with docking. control.
* Card F28388D ( www.ti.com/.../TMDSCNCD28388D) and
* TMDSHSECDOCK ( www.ti.com/.../TMDSHSECDOCK) .
Hillman Lin said: Are you using a board that is separate from your original board design for the MII loopback?
That example project works without error on our TMDSCNCD28388D controlCARD ( a Texas Instruments product ) for both the PHY that is on the…
Hi,
I checked the evaluation boards that support EtherCAT.
- TMDSICE3359
The reference clock inputs of two PHYs share the same 25MHz clock source, but the XTALIN of AM3359 does not.
- TMDXICE110
Each of the reference clock inputs of two PHYs…
Chris,
If you are starting a new project I would encourage you to move to a newer device. They have more features and are at a similar cost point. in this case they also have the additional benefit of using more modern HSEC connectors which are readily…
Part Number: TMS320F28388D Other Parts Discussed in Thread: TMDSCNCD28388D Trouble Reading Register PC: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up…