Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: TMDSEMU110-ETH , , TMDSEMU110-U Hi team,
1. Is TMDSEMU110-ETH compatible with LP-EM-CC2340R5?
2. Is TMDSEMU110-U compatible with LP-EM-CC2340R5?
Best regards,
Shunsuke Yamamoto
Part Number: LP-XDS110 Other Parts Discussed in Thread: TMDSEMU110-ETH , , ENERGYTRACE , , TMDSEMU110-U , LP-EM-CC2340R5 Hi team,
Is it possible to connect LP-XDS110 and TMDSEMU110-ETH to measure the power consumption using EnergyTrace?
Best regards,
Shunsuke…
Part Number: TMDSEMU110-ETH Other Parts Discussed in Thread: TMDSEMU110-U , TMS320F28069 Hi,
Can I use the TMDSEMU110-ETH debugger for flashing the c2000 controller family instead of
TMDSEMU110-U debugger ( currently, it is not available)
Thanks & Regards…
Alberto,
In the diagram the UART/POWER/GPIO label is showing that these connections are happening via the Target auxiliary Connection. That is done using the little breakout board that comes with the unit.
Alberto Gentile Cina said: I will only need to…
Part Number: TMDSEMU110-ETH Other Parts Discussed in Thread: ENERGYTRACE Hi,
TI provides the stune command line utility for EnergyTrace but on Windows only.
Is there a version available on Linux?
Thank you!
Part Number: LP-XDS110ET Other Parts Discussed in Thread: TMDSEMU110-ETH , ENERGYTRACE , LP-XDS110 , CC2340R5 Hi team,
My customer would like to measure the power consumption of CC2340R5 by using EnergyTrace function when the power supply voltage is 1.8V…
Hi emc_vish,
The XDS110ET LaunchPads will have the same maximum current capabilities as the TMDSEMU110-U , which is to say Energytrace can measure the consumption of a target board up to 75mA natively. With the TMDSEMU110-ETH add-on it is capable of up to…
Hi Sebastian,
The XDS110ET LaunchPads will have the same maximum current capabilities as the TMDSEMU110-U , which is to say Energytrace can measure the consumption of a target board up to 75mA natively. With the TMDSEMU110-ETH add-on it is capable of up to 800mA…
Part Number: TMDSEMU110-ETH Other Parts Discussed in Thread: TMDSEMU110-U , , ENERGYTRACE , CC1310
Tool/software: Code Composer Studio
I'm using EnergyTrace on the TMDSEMU110-U + TMDSEMU110-ETH.
After launching EnergyTrace with Run > Free Run, data acquisition…
Hello Sebastian,
The only way to change the voltage for EnergyTrace is to use an external XDS110 + the HDR accessory. These include the TMDSEMU110-U and the TMDSEMU110-ETH . Documentation for these devices are found here and more information on using EnergyTrace…