Part Number: AM2634-Q1 Other Parts Discussed in Thread: TMDSHSECDOCK-AM263 Tool/software: Hi ,
Kindly someone suggest the GPMC interface with AM2634-Q1 controller with suitable memory device of size 4MB and 8-bit data width.
Should we use asynchronous…
Part Number: AM263P2 Other Parts Discussed in Thread: TMDSHSECDOCK-AM263 , SYSCONFIG Tool/software: Hello E2E Experts,
Good day
am attempting to increase the number of PWM pins available to me on the AM263Px control card EVM through the use of pin…
Part Number: AM2634 Other Parts Discussed in Thread: SYSCONFIG , , TMDSHSECDOCK-AM263
Tool/software:
Hi
Based on the " TMDSHSECDOCK-AM263 ", it is shown the compatible flash/SRAM devices include 256 Mb device.
But as per SysConfig tool the address…
Hi Dan,
TMDSHSECDOCK/ TMDSHSECDOCK263 is used for breaking out the 180-pin HSEC connector (present in the controlCARDs) to the headers present on it. In TMDSHSECDOCK263 (for AM263 controlCARD), it conditions some additional hardware to support the peripherals…
Part Number: AM263P4 Other Parts Discussed in Thread: TMDSCNCD263P , TMDSHSECDOCK-AM263 , TCA6424 Tool/software: Hello,
I am using the AM263Px Control Card (TMDSCNCD263P) along with the AM263x controlCard Dock (TMDSHSECDOCK-AM263). I am attempting to…
Hi Bivin,
For flash devices, please see the AM263x Flash Selection Guide .
For an SRAM example, please see the TMDSHSECDOCK-AM263 , which is equipped with a 64Mb PSRAM device for interfacing with the AM263x GPMC peripheral.
Regards,
Brennan
Part Number: MCU-PLUS-SDK-AM263X Other Parts Discussed in Thread: SYSCONFIG , TMDSHSECDOCK , TMDSHSECDOCK-AM263 Hello all,
I have changed "mcan_loopback" example from SDK and disabled internal loopback so that I can see transmitted data on MCAN_TX.…
Hi Sadaiyandi, I have made the changes you mentioned. Btw I am using this HSCEDOCK: https://www.ti.com/tool/TMDSHSECDOCK-AM263 as it has an onboard transceiver connected to MCAN0.
I am able to observe pulse at MCAN0_TX signal when I probe pin 1 according…
Part Number: TMDSCNCD263P Other Parts Discussed in Thread: UNIFLASH , TMDSHSECDOCK-AM263 Tool/software: This is my first question. I bought TMDSCNCD263P and am trying to flash it by watching the academy. I was able to flash using the command prompt. However…