Part Number: TMDXEVM438X-EPOS Hi,
Can anyone suggest where to download SDK for
TMDXEVM438X-EPOS EVM board.
When i cliked on securesoftware link, following message was displayed.
You do not have any secure resources
Part Number: TMDXEVM438X-EPOS
Hi TI Team,
I am working on TI 438x processor board (TMDXEVM438X-EPOS). And it is running on linux os.
I want to make this board as a usb device and want to implement usb vendor class on it.
So how can i achieve this…
Part Number: TMDXEVM438X-EPOS
Hi,
I'm interested on using the AM438x for a low power application. The processor will be in suspend to RAM state most of the time. During this state, I would like to have the PRUs collecting and writing data to memory…
Part Number: AM4372 Other Parts Discussed in Thread: TPS65218 , TPS65218D0 , TPS65910 , TPS65217 , TPS650250 , TPS6521825 , TPS6521815 , TMDXEVM438X-EPOS , TMDSEVM437X , AM5728 , AM4378
Hi TI Experts,
I am working on a design using AM437x or AM438x…
Part Number: TPS65216 Other Parts Discussed in Thread: TMDXEVM438X-EPOS , TMDSEVM437X Tool/software: Hello, In datasheet, DCDC1 and DCDC2 are described to have max output capacitance of 100µF, but accepting a 500µF remote capacitance. Can you detail what…
Part Number: TIDEP-0093 Other Parts Discussed in Thread: TMDXEVM438X-EPOS In my company, we're using AM43-EPOS-EVM based POS terminals. Right now, our payment terminal vendor provides firmware with the Linux kernel 3.14.43 version. I'm wondering if TI…
Hello,
It is still recommended to have a local 47 uF capacitor placed near the pin of the TPS65218D0,
At the points of loads, a certain level of remote capacitance, above the maximum local capacitance amount, is okay on DCDC4. DCDC1/2 specifically…
Part Number: TCA5013 Other Parts Discussed in Thread: TMDXEVM438X-EPOS Hello TI,
I am looking for software library associated with TCA5013 module and also please suggest a EVM which provides the Proof of concept for the same.
Thank you
Part Number: TPS65218 Other Parts Discussed in Thread: TMDXEVM438X-EPOS , , Hi,
In the TMDXEVM438X-EPOS, all inputs of TPS65218 are supplied from VBAT.
So 220uF is adopted and there is tantalum capacitor.
Is it correct?
if MLCC, 16V, 20% is adopted…
Part Number: AM4372 Other Parts Discussed in Thread: AM4382 , AM4378 Hi TI Team,
I am working on TI 438x processor board ( TMDXEVM438X-EPOS ). And it is running on linux os. Due to security reason i have to put part number am4372, I think for usb class…