Part Number: TMS320DM8148 Hi,
We are currently working to increase the reset pulse width output from the TMS320DM8148 - RSTOUT_WD_OUT pin to meet our goal of >1us.
Currently, BTMODE[11] is tied to ground, and we have attempted to modify the PRM_RSTTIME…
Part Number: TMS320DM8148 Tool/software: Im using in my product the TMS320DM8148 C CYE2. Is it possible to use the TMS320DM8148 S CYE2 instead.
What are the differences? Are the two chips pin compatible?
Part Number: TMS320DM8148 Hello,
We are currently designing with the TI TMS320DM8148CCYE1 processor and using Micron MT41J128M16JT‑125:K (1.5 V DDR3) , which is now going EOL. We are evaluating DDR3L (1.35 V) memory devices as potential replacements…
Part Number: TMS320DM8148 Hi,
I am looking for SOC's available from TI family which can be used for IP camera products. Please share the list and where on TI I can look for its specification & datasheet.
Thanks.
Part Number: TMS320DM8148 Hi Dear Forum members
we are massively using the TMS320DM8148 in several products
the the boot load we are using normally is: SPI --> MMC -->UART --> EMAC [BTMODE(4:0) --- 10110]
the boot load files are located at the MMC…
Part Number: TMS320DM8148 Tool/software: Hello,
To sleep our LCD monitor, I need to disable or keep ACTVID signal off during LCD sleep as LCD monitor vender requires.
As far as I checked Technical Reference Manual of TMS320DM814x, it seems the DVO_OFF…
Other Parts Discussed in Thread: TMS320DM8148 , Z3-3P-VIDEO-EVMS Is TMS320DM8148 still available? Which development board is the most complete for TMS320DM8148?
Also, is Z3-3P-VIDEO-EVMS still available? Because Z3-3P-VIDEO-EVMS is not found on the…
Part Number: TMS320DM8148 Hi
I am operate the VPDMA, I am using version 1AD for the VPDMA_firmware.
base on SPRUGZ8G from 14 November 2011 revised 2016
if I understand the Datasheet
BIT RDY VPDMA-list_attr should mark that I can reload or load…
Other Parts Discussed in Thread: TMS320DM8148 , AM5728 Hello.
I need the article:
https://processors.wiki.ti.com/index.php/EZSDK_Memory_Map
Where can I find it?