Part Number: TMS320F28067 Hi,
We faced one issue about ADC accuracy, the same configuration, with only one difference on register ADCINTSOCSEL2.
When ADCINTSOCSEL2=0, SOC8's accuracy is not good. When keeping the value ADCINTSOCSEL2 after offset calibration…
Part Number: TMS320F28067 Hi,
Customer has some questions about read/write of memory addresses:
1) If the code read an address, which is in "reversed" area, what will happen? For example the address is 0x3D7D00.
2) If the code read an address, which…
Part Number: TMS320F28067 Hi,
Customer is using F28067 for their application. There's one bit in RAM 0x1214C (L8), which is not writable. The bit is number 8.
For example, code tried to write 0x1111 to the RAM. After writing, value 0x1011 was read…
Thanks Vivek, I will do that. Also, because the pins only need to be connected together during debug, I can leave those resistors unconnected for production boards, so such problems will not appear on them.
Regards,
Jouko
Part Number: TMS320F28075 Other Parts Discussed in Thread: TMS320F28067 Hi Team,
As shown in the picture, the technical manual didn’t mention that 075 Data must be sent in 16-bit mode with FIFO enabled. But in real tests, when I set SPICHAR=F, the master…
I need a letter of volatility (LOV) for this part. It should look like the attached. The letter will describe the memory on the part, its function and how to sanitize it.
Can you provide an LOV for this part?
Statement of Volatility_TMS320F28069_68_67…
Other Parts Discussed in Thread: TMS320F28067 I'm using Piccolo DSP TMS320F28067.
I would like to use RS-422 receiver for SSI interface. \
Can I use the SN65C1168PW which has Voh of 4.2V and connect it directly to SPI MISO pin at the DSP (4.6V is…
Part Number: TMS320F28386D Other Parts Discussed in Thread: C2000WARE Hi C2000 Champ !
As I checked the availability via C2000-IEC60730-SW-PACKAGE page. I am not able to find TMS320F28386x device in the list.
Can you please clarify if TMS320F28386x…