Hi Matthew
Thank you for your reply.
Re. Q1) I was load to flash regions. Re. Q2) My CCXML file select connection is "Texas Instruments XDS100v2 USB Debug Probe" and select Board or Device is "TMS320F28075", others setting not to change. Do I have…
Part Number: TMS320F28379D Tool/software: Code Composer Studio Hi,
I have two questions to ask. Q1.
I am using F28379D controller to generate PWM signals for my three phase inverter. But the PWM method I am using requires to XOR three PWM signals…
Part Number: OPA365-Q1 Pl ignore the first pdf attachment. Got in by mistake.
Pl see attached approach to non-dissipating current sense using NVE sensor. This requires the selection of opamps appropriately.
Will appreciate any suggestion to make the…
Part Number: TMS320F28379D Other Parts Discussed in Thread: C2000WARE Tool/software: Code Composer Studio What are the minimum changes needed to execute code from flash? (no reading/writing data from the executing code to/from flash)
In the flash_programming_cpu…
Part Number: TMS320F28379D Hello Experts,
I am using F2879d for implementing my Boost PFC Hardware. I have taken the Plant transfer function from literatures and i used MATLAB control loop designer tool to obtain my PI parameters. I got my Kp Ki for…
Part Number: TMS320F28379D Other Parts Discussed in Thread: TIDM-1000 , CONTROLSUITE Tool/software: Code Composer Studio
Dear Sir,
When I am working with the example TI Designs: TIDM-1000, I am not getting the PWM Gate pulse like above shown in pdf…
Part Number: TMS320F28379D Other Parts Discussed in Thread: C2000WARE Tool/software: TI C/C++ Compiler Hi,
My client plans to run 4x 16 bit ADC at the same time at max 1Msps for 8k sample points, and do DFT/FFT on collected data.
I have some questions…
The signals i'll reply for you within tomorrow but I don't understand what do you mean "set GPIO61 to a GPIO but then set it back to the hardware SPI CS" Which line It's set back to GPIO? I
I use a original code but it set SPI-C so I need to change…
Part Number: TMS320F28379D Hello,
This is regarding PWM application same as the previous post.
In the previous post, ADC ISR is implemented in CLA side, this time it’s in C28x side.
Please see below screenshot.
Q1. When PWM duty is 0…