Is there a power spreadsheet for the VC5416 DSP? I know the power spreadsheets exist for a few of the other processors. Can you let me know?
Thanks Charles
Other Parts Discussed in Thread: TMS320VC5416 Hi,
will you please send me how to work the echo program given by texas.it will be very helpful for me.
with regards,
sharmi
Other Parts Discussed in Thread: TMS320VC5416 Hi!
Can we decrease the core voltage of TMS320VC5416/160MHz DSP if we apply lower clock frequency. The specified core voltage is 1,6V for 160MHz CPU version and 1,5V for 120MHz version. Can we apply 1,5V…
I am trying to port some 5416 code developed using CCS3.1 into CCS V5.1. I have selected Family C5400 and Variant is Generic C54xx device in the project build options, and also in Compiler Runtime Model Options I have checked Use Far Calls. The compiler…
Hi,
I want to do echo program in realtime,first i have decided to generate voice. i can hear the voice through the speaker but with noise,i want to remove the noise
what my doubt is whether i have to add any external circuit or by means of software…
Hi,
I am new to the dsp5416,Will you please send me the program for echo generation and cancellation to work in realtime.It will be very helpful to finish my project.
Regards,
Newla Blessie.
Steve,
The TMS320VC5416 does not have a USB digital core on-chip and therefore the TUSB1105/6 are NOT an option to be used with it. They are only transceivers and need the attached processor to integrate the digital core to enable USB functionality…
Other Parts Discussed in Thread: TMS320VC5416 Dear Friends,
I have a TMS320VC5416 Based board which i need to program for IO space.
The interface has following signals connected with an on-board CPLD:
1. D15-D8 (8-Bit Databus)
2. A7-A0 (8…
Other Parts Discussed in Thread: TMS320VC5416 Hi,
I am working with TMS320VC5416. I want to use external interrupt INT0, INT1, INT2.
I have check my code in simulator, when I set the IFR bit '0' (IFR = 0x0001), it does not jump to ISR. It jump…
Other Parts Discussed in Thread: TMS320VC5416 Hello! I'm having troubles with emulator xds510 usb 2.0 I've made boards for two processors: TMS320VC5416 and TMS320R2812 (Texas Instruments). I've installed all the drivers according to datasheet and I'm…