Part Number: TMS470R1A256 Hi,
How do you flash the TMS470R1A256 micro? What hardware tool do we use to read the already existing HEX file and then flash it?
Thank you.
Part Number: TMS470R1A256 Hello,
The current product developed 10 years ago and used TMS320VC5471ZHK on its control board. It was a multicore DSP including one C54 DSP and one ARM7TMDI MCU. In TI website it is not recommended for new design. The original…
Part Number: SM470R1B1M-HT Other Parts Discussed in Thread: TMS470R1A256 Tool/software: Code Composer Studio Code composer does not seem to support either the SM470R1B1M-HT or the TMS470R1B1M-HT. Is there another device install package to add support for…
Thank you.
T
These are my project file properties in CCS3.3.
When I chose device in CCS6, TMS470R1A256 was chosen.
But it can't pass the connection test.
Is my XDS100V2 damaged?
Do I choose the wrong device?
Thank you.
Other Parts Discussed in Thread: TMS470R1A256 Hi there,
Hi I have a problem using the Spectrum Digital XDS510 USB emulator. When trying to connect to a target (ARM7) this is what i get:
Error connecting to the target : Error 0x80000244/-2131
Fatal Error…
Other Parts Discussed in Thread: SM470R1B1M-HT , TMS470R1B1M , TMS470R1A256 Hi,
I am planning to use SM470R1B1M-HT microcontroller in my new design for high temperature applications. I tried with Code Composer Studio by installing free version, I couldn…
Other Parts Discussed in Thread: RM48L952 , SEGGER , TMS470R1A256 , ATOLLIC , TMS570LS20216 , HALCOGEN Hello.
How can I debug RM48CTRLCARD using GDB? I want to use JLinkGDBServer because of beta JLink driver is badly working in CCS5.4.
I set up debug configuration…
Other Parts Discussed in Thread: TMS470R1B1M , TMS470R1B768 , TMS470R1B512 , TMS470R1A256 , TMS470R1A288 , SM470R1B1M-HT Hi team,
In looking at the TMS470 Hercules processors, they're storage temp is rated to -65C.
1) Is there something specific to the…
Other Parts Discussed in Thread: TMS470R1A256 Hi
I have a tms470r1a256 board successfully connected to CCS3.2 using xds510.I have a simple project ready with memory remapped to entire RAM section in the linker cmd file.
ram sections relocated map:- …
Other Parts Discussed in Thread: TMS470R1A256 , TMS470R1B1M , SM470R1B1M-HT Hi-
I'm tyring to find an up to date flash api that will work with a TMS470R1B1M (or TMS470R1A256) and IAR embedded workbench v5.5. It doesn't seem that the "TMS470/570 Platform…