Hi Ece dogan,
The product page link was not updated with new version of certificate, we will correct it.
Mean time you can access the updated certificate from here:
TMS570LS31_21_IEC61508_ISO26262_Certificate.pdf
-- Thanks & regards, Jagadish…
Hello Rony,
Our MCAL supports the modules in TMS570LS3135 and TMS570LC4357 devices, but doesn't support RM4x devices.
The latest version MCAL (6.0.0) drivers support AutoSar 4.0.3 and 4.2.2. TI does not charge for those Hercules MCAL releases.
Part Number: TMS570LS3137 Other Parts Discussed in Thread: HALCOGEN , TMS570LS3135
Hi, in halcogen there are two variants of ls31x which have freeRTOS support. I want to port freeRTOS from these variants to ls31x USBStick.
I know, firstly I have to…
Tom,
Typically these are in the product folder for the device you are using. For example:
http://www.ti.com/product/tms570ls3135
In your case, I don't see that particular device folder on the web yet, so I will request.
Regards,
Aaron
Yes. I've searched on TI website.
I saw Uniflash and XDS100 might be my best choice. But their supported processor list only includes up to TMS570LS3135. Does not have LS3137.
I guess it's not updated to the latest in time, so I want to get confirmed…
Other Parts Discussed in Thread: TMS570LS3135 , TMS570LS3137 Tool/software: Code Composer Studio Hello there,
-> For the screenshots please see the case CS0037980:
warning #10247-D: creating output section ".sysmem" without a SECTIONS specification…
Hi Nomoto,
The TMS570LS3137 and TMS570LS3135 both do include RTP and DMM modules. You may refer to the Datasheet and Technical Reference Manual at the links below for details on how to use these modules.
TMS570LS3137: http://www.ti.com/product/TMS570LS3137…
Other Parts Discussed in Thread: TMS570LS3135 I'm looking at the document SPNS164 - September 2011 for the TMS570LS3135.
In section 5.3 it says "The GPIO module on this device supports two ports, GIOA and GIOB.", but when I look at section 2.2 - the…
Andy,
The only difference between TMS570LS3135 and TMS570LS3137 is that TMS570LS3137 has Ethernet. So, they both have 2 SCI/LIN modules on them. The SCI can be used as a UART. So, you will be able to do RS232 on one SCI/LIN (using just the SCI features…
Part Number: TMS570LS3137
Hi ,
Attached Failure log of the Lauterbauch and TMS570LS3137 Lauterbauch script
I am using Lauterbauch script to load .out file generated from our project .
there is ECC section in our project so the .out file contains…