Other Parts Discussed in Thread: TMUX1209 , TMUX6209 , TMUX7209 Hi,
Good Day. I have a customer who wants a CAN Switch IC. I hope you can help him to find one that fits for his wants. Please see below his query for your reference. Thank you very much…
Part Number: CD4053B Other Parts Discussed in Thread: TMUX6219 , TMUX7209 , TMUX6211 Hello team,
I received a question from my customer about the specifications of the CD4053BPWR.
They would like the output signal to have a fall time of 400ns when…
The following table helps select th e right multiplexer and switch with Mid Voltage 25V =< VSIGNAL =< 99V in different configurations:
Precision , Protection , Automotive , Extended Temperature
Configuration
16:1…
Hi Ryoma,
the maximum supply voltage of OPA2991 is 40V and a special protection circuit against too high differential input voltages is used:
1778.sbot040c.pdf
The TLV9152, on the other hand, has a maximum supply voltage of "only" 16V and can withstand…
Hi Corbett,
the footnote (4) in the absolute maximum ratings seems to indicate the presence of a protection scheme against too high differential inputs voltages, similar to what is used in mux-friendly OPAmps:
sbot040c.pdf
This can be responsible…