Part Number: TPA3116D2 Tool/software: Hello,
My input is a continuous sine signal, and I only control the MUTE pin to loop and achieve playback for about 300ms and mute for about 30ms. Discovered a POP sound issue with the speaker. The circuit diagram…
Part Number: TPA3116D2 Tool/software: I'm only getting output when the PLIMIT and RINN pins are shorted, but the audio is distorted and the IC becomes very hot.
Could you provide the correct voltage levels and connection details for the PLIMIT, GAIN…
Part Number: TPA3116D2EVM Tool/software: Hi,
Can we use this EVM to generate frequency of about 5Hz. Also could you say what is the frequency response of this EVM
Part Number: TPA3116D2
Tool/software:
Hello, In the Audio input section the gain =36dB, input impedance =9k ohm and Ci (input cap) = 1uF (for a flat bass)
as per datasheet 7.3.7, RC time constant should be 1ms or lesser to avoid POP sound where…
Part Number: TPA3116D2 Tool/software: Class D Amplifier.pdf
I have a schematic here I would like to get checked for any glaring issues. By my calculations PVCC should be 18V, and VCC is ~12V coming from a 3S2P lithium ion battery pack. I am nervous…
Part Number: TPA3116D2 Tool/software: I am facing to pass the BCI tests while using this amplifier board. Noise getting between 20 mhz to 200 mhz.
Can you please someone guide to me how to resolve this issue
Part Number: TPA3116D2 Tool/software: Dear team,
Would you please recommend the best solution for piezo driver? I already know TI has "piezo driver" portfolio but also believe audio power amps like TPA3116D2 can be used to drive piezos.
Below is the…
Part Number: TPA3116D2 Tool/software: Hi E2E Team,
We are currently using the TPA3112D2-Q1 in our design with the following configuration:
Modulation Mode: BD
Output Configuration: BTL(Right channel used, Left channel unconnected)
…
Part Number: TPA3116D2 Tool/software: Hi,
Please kindly review the schematic diagram for TPA3116D2.
BTW, please advsie if we can use the single-ended input in the PBTL, thanks.
Part Number: TPA3116D2 Tool/software: Hello,
I'm building an amplifier based on TPA3116D2 in PBTL mono configuration.
I would like to drive a 6ohm sub-woofer, rated 120W.
I'm going to use a 24V supply.
From figure 22 and 26 of datasheet I can…