Hi Mathew,
1. Referencing "Figure 2: TPA3116D2EVM Schematic" on the datasheet, I'd first jump (short) C1, C2, C3, and C4 to allow DC to pass to the inputs of the TPA3116 IC.
TI: TPA3116 input is biased at 3V, so the DC blocking cap is necessary. Our…
Part Number: TPA3116D2EVM I am having an issue with the frequency response of this amplifier. I tested the frequency response using a 70 mV rms single ended input signal from 256Hz to 200kHz, with a 24V rail voltage at 1.2MHz switching frequency. I have…
Hi Shawn
Thanks for the explanation.
Curious how you came to terms that my application should not be a problem? Output = 11Vrms & Load = 3Ohm (2x 6 ohm in parallel) ...40W right?
How does the power supply effect the maximum output? If I limit it…
Hi Shawn,
could you please help me to find the right TI FAE contact who can support me on this issue? I couldn't find any information on your website and I wrote a few emails to FAEs that are known in my area (Germany) but I didn't get any responses…
Part Number: TPA3116D2EVM Can I get some help in trying to get your EVM board to operate properly in PBTL mode. I have tried two units so far and when as configure as the User Guide instructs all I get is a a pulsed DC offset on the outputs.
Thanks…
Part Number: TPA3116D2 Dear TI Support,
I am currently evaluating the TPA3116D2EVM with a 24 V power supply.
I would like to ask about the TPA3116D2:
I could not find a clear specification in the datasheet regarding the input voltage range for the…
Part Number: TPA3116D2
To: TI Support
I have a question regarding the following application note: “Guidelines for Measuring Audio Power Amplifier Performance”
In Section 4.4 (Maximum Input Voltage), is the following interpretation of the formula…
Part Number: TPA3116D2 HI team,
Can I combine multiple tpa3116d2 available modul into one?
Can I use two mono TPA3116D2EVM board to achieve 200W output?
Description of TPA3116D2EVM
"the evaluation module can also be configured as a 100-W, Class…