Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 Tool/software: Hello
looking for application note for TPA3255
we would like to have one MONO Audio input and parallel load for 300 watt on 6 OHM speaker
we would like to get the full…
Part Number: TPA3255 Hi team,
The datasheet says ±3.9V peak max is possible in "Typical Applicaations" section, but I believe this would violate the absolute maximum ratings of the INPUT_X. Could you clarify what the actual input range is ?
From…
Part Number: TPA3255 need advise , my test from my TPA3255 amplifier condition with resistor 4 ohm load. picture attach is distortion capturing waveform and nondistortion
Part Number: TPA3255 Hello
I have two questions regarding the efficiency graph for TPA3255. 1. I would like to see a graph of THD + N = 1%(BTL). If this graph is not available, how can it be expected to change ? I would like to get a general image.…
Part Number: TPA3255 Tool/software: Hello, good morning! I need a help whit TPA3255 (Schematic ZK-3002). I would like some technical information about the TPA3255. Here is the layout scenario: Four amplifiers (TPA3255 (PBTL MODE) (ZK-3002)) with their…
Part Number: TPA3255 Tool/software: I have been reading through this document: https://www.ti.com/lit/an/slaa701a/slaa701a.pdf?ts=1739782374813&ref_url=https%253A%252F%252Fwww.google.com%252F
and it seems there is no way to get rid of Ripple Voltage…
Part Number: TPA3255 Tool/software: Hi TI,
I have designed a Class D 240W audio amplifier with TPA3255 in PBTL configuration. I have used two test conditions to measure the power dissipation of class D IC as follows
• Case 1
Vin - 52V
Iin - 6…
Part Number: TPA3255 Tool/software: Hi All
Working on a prototype TPA3255 amplifier.
I wanted to use a T106-2 core (2 for stereo) winding both coils for the BLT mode on one core.
the coils are wound tightly together, and connected opposite to…
Part Number: TPA3255 Tool/software: Hello,
The customer uses TPA3255 to drive the motor coil. The schematic diagram is shown below. Customer feedback: The chip heats up severely and produces a lot of noise. The motor speed is not sufficient compared…