Part Number: TPA6404-Q1 Other Parts Discussed in Thread: TPA3116D2-Q1 , OPA1678 Hi Team, We are currently developing an infotainment system based on the NXP MIMX8ML6CVNKZAB processor and would like your support in reviewing our audio architecture and…
Part Number: TPA6404-Q1 Tool/software: Hi team,
Currently, our diagnosis involves reading the values at addresses 0C and 0D, with the condition that the value at address 0F becomes high-impedance before reading;
We would like to confirm whether there…
Part Number: TPA6404-Q1 Tool/software: Hello,
I wanted to inquire if the TPA6404-Q1 amplifier supports a 100W output , specifically 25W per channel across its four channels. Additionally, we are planning to interface this amplifier with a processor…
Part Number: OPA1678 Other Parts Discussed in Thread: TPA6404-Q1 , TPA3116D2-Q1 , , TPA3116D2 Hi Team, We are currently developing an infotainment system based on the NXP MIMX8ML6CVNKZAB processor and would like your support in reviewing our audio architecture…
Part Number: TPA6404-Q1 Tool/software:
Hi Audio Experts!
I have some technical questions about designing the output filters for Class-D amplifiers.
We are using this components at the output channel.
Do you have any information(application…
Part Number: TPA6404-Q1 Tool/software: Hi Team,
We are currently developing an infotainment project based on the NXP MIMX8ML6CVNKZAB processor and have implemented the following audio architecture:
Codec: TLV320AIC3104IRHBR
Amplifier: TPA6404QDKQRQ1A…
Part Number: TPA6404-Q1 Hello,
I requested full datasheet from TI request page of TPA6404-Q1 but I could download PurePath software only.
Could you send me complete datasheet ?
And why is complete datasheet not published on web page?
Regards…
Part Number: TPA6404-Q1 Hello,
My customer is asking about TPA6404-Q1 at PBTL mode
In this mode, can it output 60W power with below conditions?
Conditions:
DC supply(PVDD) : 12V 、
Speaker: load 1 Ω (Mono) ( 0.8 Ω min. )
Output : 60W Max…
Part Number: TPA6404-Q1 Hi Expert,
Our customer want to use TPA6404 to driver Linear amplifier and speaker at the same channel. To sum up, the load is two 4ohm speaker + linear amplifier. The channel works under speaker mode. They don't the detail about…