Hi Team,
Is there any difference between Dx+ pin and Dx- pin? I consider to connect Dx+(Dx-) pin to Dx-(Dx+) of display port signal. I believe it is no difference between these pins.
Best Regards, Yaita
Other Parts Discussed in Thread: TPD8S009 HI,
I've been using the TPD8S009 ESD protection for DisplayPort applications running at RBR and HBR for a while.
Does this device also support the HBR2 (5.4 Gbps) bandwidth?
Best Regards,
Marco
Other Parts Discussed in Thread: TPD2E009 , TPD8S009 Team,
Customer is using the Aria II GX transceivers at 3.75Gbps. Will the TDP8S009 work at this speed? I've also shown the TPD2E009 but they prefer a multi-channel device. Please let me know or make…
Back to Interface Home Page
DisplayPort Protection
Highlights:
Data speeds up to 20Gbps
8 data lines, 20 total pins
3.3V, 500mA Input
Low capacitance required on data lines
Device
V RWM
Cap
(pF)
ESD(kV)…
Part Number: TUSB1046EVM Other Parts Discussed in Thread: TUSB1146 , TPS65982 , TPS65987D , , TPS65988 , TUSB1064 , TPD4E05U06 , TPD8S009 , TPD4S010 Hello~
I'll attach the circuit I made and the project file.
My purpose is monitor output through…
Hi Gerasimos-san,
Thank you for your response.
I have already suggested TPD8S009 to our customer as I found the following post, so should I suggest TPD4E02B04 again ? In addition, is TPD8S009 not reasonable for this application ?
Does TI have eDP…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…
Hello Nam
As you can see in the part of Features, this device works with AC-coupled TMDS or DP++ (it means that this device can handle AC-coupled TMDS and DP) to HDMI 2.0. Then, if you have from you GPU (Jetson) a DC-coupled TMDS signal, then you'll…