Other Parts Discussed in Thread: TPL0202-10 Hi team,
Could you tell me what the alternative to the following product ?
・Microchip MCP4362T-503E/ST
Best Regards,
Tomoki
Other Parts Discussed in Thread: TPL0202-10 Hi,
can you confirm TPL0202-10 EEPROM read cycles is really as low as 1000 at 85C? TPL0102 as comparison specifies an endurance of 100,000.
Thanks, KF
Hi Giovanni,
We have not implemented any impedance control in this design.
The digital potentiometer determine the two thresholds of the two comparators in the board. The value of these two threshold depends on what you are trying to achieve with your…
Other Parts Discussed in Thread: TPL0202-10 , MSP-GANG Hi!
Our customer will use TPL0202-10 device.
Asyou know, TPL0202-10 device is SPI interface. But System of our customer don't have MCU.
So, Our customer want GANG Progrmmer information.
1. Can you…
Hi Red,
We have two DPOTs with nonvolatile memory:
http://www.ti.com/product/TPL0102-100
http://www.ti.com/product/TPL0202-10
We are also going to APL a low cost DAC with NVM as well. Please email me if you are interested in promoting that device to your…
Hey Aldo,
We recommend using a TI digital potentiometer such as the TPL0102-100 ( www.ti.com/.../tpl0102-100) or TPL0202-10 ( www.ti.com/.../tpl0202-10) for either I2C or SPI control, respectively. Place this digital potentiometer in place of the top feedback…
Hi Joaquim,
Not sure I understood your question but it is possible to request samples or order the TPL0202-10 through TI store www.ti.com/.../samplebuy
Thanks
Giovanni
Hi Kaue,
Welcome to E2E and thank you for your query. The TPL0401A-10 cannot support your requirement as the difference between the pins H and W cannot be negative. You can look at TPL0202-10 - it can support this mode as long as all pins H, L and W…
Other Parts Discussed in Thread: TPL0202-10 Hello there
I have one question about datasheet.
When I check TPL0202 datasheet 17page, there is DPOT table.
In table, each RHW and RWL has maximu resistor is 100K ohm, is it right or typo?
I think it should be…
sir,
The datasheet of the TPL0202 digital potentiometer table (page no-17) shows that the end to end resistance value is 100 K. But, actual resistance is 10 K.