Part Number: TPL5010 Hello,
The timing interval setting for TPL5010 is shown in the schematic diagram and should be 15 seconds. The actual testing time interval by the customer is not accurate. The actual testing time may be 15s, 16s, 17s, 18s, 19s…
Part Number: TPL5010 Other Parts Discussed in Thread: SN74LVC2G08 I am designing an ultra-low power battery-operated IoT device and I plan to use the TPL5010 as a system wake-up timer. To conditionally enable or disable the timer based on specific hardware…
Part Number: TPL5010 I want to use TPL5010 as a watchdog incase of continous off state of SBC. I am using only done and rstn pin;done to receive done msg from SBC if it in normal state(ON),whereas rstn pin to force ON the SBC by pulling pwr_btn of SBC…
Part Number: TPL5010 Tool/software: I am using the TPL5010 in a new design the wake drives an interrupt in the CPU and the CPU responds with DONE. For some reason the wake pulse does not seem to be happening. Every 90 minutes as set by the timing resistor…
Part Number: TPL5010
Hi Team,
Posting on behalf of our customer.
I'll share this E2E post with our customer so he can reply when needed.
We are experiencing an issue with the TPL5010 watchdog timer and would appreciate any assistance.
…
Part Number: TPL5010 Tool/software: Dears,
1. My customer uses TPL5010 in a new project. According to the data sheet, the recommended resistance value for 50S is 20.047K. However, according to the given formula 1, it should be 20.47K. Is this a problem…
Part Number: TPL5010 Tool/software: Hi. I'm Jussi Hakulinen from Finland.
My aim is to use TPL5010 as watchdog for Linux system,
Is it possible to use two separate timebases? For example first 60sec timeout for program loading and then normal operation…
Part Number: TPL5010 Other Parts Discussed in Thread: TPL5110 Tool/software: Hi. Many thks. Is the following case possible? To use two pcs of TPL5010. Very economical and flexible component. Remarks (schematic attached): 1) For watchdog timer use - can…
Other Parts Discussed in Thread: TPL5010 , TPL5111 Tool/software: I want to create a 60Hz pulse signal using an ultra-low power consumption IC.
In the following thread, in response to a question about creating a 20-40Hz pulse signal, the answer was…
Part Number: TPL5010 Tool/software: Hi all,
This is Arabella, the FAE from NWC MM team. Now my customer used TPL5010 to data exchange project. There are 4 questions they want to know:
1. The customer did not use WAKE, and gave several high levels…