Part Number: TPL5110 Hello
I need to blink the LEDs every second when power is applied.
Is it possible to use the DRV output as a load for an LED?
Is the circuit below correct?
Part Number: TPL5110 Other Parts Discussed in Thread: TPL5111 , SN74LVC1G11 , SN74LVC1G80 , SN74LVC1G3157 Hello.
Please tell me if the circuits are designed correctly In Figure 1, I would like to design the TPL5110 to start a timer by pressing a button for…
Part Number: TPL5110 Hi, Just trying to understand the wording on the data sheet, is 100nsecs the minimum time that DRV takes to respond to the done input signal, or does there have to be a delay of 100nsecs after DRV before done can go active.
Part Number: TPL5110 What happens if the Manual On is held HIGH while the DONE pin is triggered? Say the time period is set for 5 seconds. The Manual On is held from second 0 to second 4. The Done signal is sent at second 3.
Part Number: TPL5110 In One Shot mode, what happens if the Manual On (ie DELAY pin goes High) while the DRV pin is already active (ie DRV is low and the MOSFET is on)
Part Number: TPL5110-Q1 Hi Team,
I am considering to use a TPL5110-Q1 for power saving, by enabling the main 5 V supply through a pMOS around every second (tIP–50 ms).
I would connect the DONE pin to ground, and the DRV pin to a nMOS that switches…
Part Number: CSD25501F3 Other Parts Discussed in Thread: TPL5110 , Tool/software: We are designing a new battery powered circuit using TIs TPL5110. I need to find a MOSFET for the design and to determine the leakage current Idss for battery lifetime estimations…
Part Number: TPL5110 Hi Team,
My customer is evaluating our TPL5110 at the timer mode, but also will use the manual power ON by the M_DRV pin, so according to the datasheet fig.11, there is a question below and need your kindly help to check that:
If…
Part Number: TPL5110 Hi Team
Good day
My customer want some help:
I'm looking for a timer product with a function to turn off automatically after 90 minutes. i want to know if TI has any part with function like IC BU2305 (RoHM).
Can IC xxx be functioned…
Part Number: TPL5110-Q1 Hi all,
I got a question of TPL5110-Q1 how to set the time interval of mid value between two values in the lookup table, e.g. 130ms. I don't think this is feasible but can you tell me if this is feasible using this device?
…