Part Number: TPLD1201 Tool/software: Hi team,
Once the OTP memory of the TPLD1201 is programmed using InterConnectStudio, it becomes a permanent program and cannot be rewritten. Is this understanding correct?
During the design phase, you are configuring…
Hi Abel,
This would require you to go into the ngspice.xdt file and make some changes, namely delete the highlighted portion below (as you can see I ctrl+f searched for "Unahndled output" to find these lines):
The ngspice.xdt file is found in C…
Hi Malcolm,
You wrote: (red text)
Could you see what happens if you connect the input of pin IO7 to a couple of different things, such as VCC, or POR? If possible, it would also be helpful to test this normal case while connecting POR to a separate…
Part Number: DS90UB913A-Q1 Hello,
There is a phenomenon that the PCLK changes by changing the GPO pin [1: 0] of the DS90UB913A-Q1 in the customer.
They created a program that intentionally changes the state of GPO [1: 0] in about 0 ms to 2 ms after…
Part Number: DS90UB949A-Q1
・DS90UB949→DS90UB948へのFPD-Link III高速シリアル転送を行う際には、制御用としてデータシート8.3.9 Back Channel Data Transferに 記載されている双方向の通信は必須でしょうか?それとも、双方向の通信を行わずにDS90UB949→DS90UB948の通信のみを実行する ことは可能でしょうか? ・(上記双方向通信が必須の場合)、この通信で使用するピンを教えてください。
・データシートに8B10Bの説明が見つかりません…
Hi Tiger,
I have attached a UB941AS datasheet with the package dimensions. I'll look into why the package dimensions aren't available on TI.com.
Best,
Jack
ds90ub941as-q1.pdf
Part Number: DS90UB949-Q1 Other Parts Discussed in Thread: ALP Serializer:DS90UB949 Deserializer: DS90UB 948 Number of Pixels: 1920 × 720 × 60 H z × RGB
The screen parameters and some configuration param 仪表串行器TI949 730002187_ds90ub949-q1.pdf snla132g…
Part Number: DS90UB913Q-Q1 Other Parts Discussed in Thread: DS90UB914Q-Q1 Hi, Team
An automotive camera and SRV customer start using DS90UB913Q-Q1 from 4 years ago. They use "PCLK from imager mode". Accroding to DS90UB913Q-Q1 datasheet "SNLS420B", the…