Part Number: TPLD1201-Q1 Hello,
I require a rising-edge retriggerable pulse detector with the following functionality:
When a rising edge is detected on the input pulse, the output should go HIGH and remain HIGH for 800 ms.
If another rising…
Part Number: TPLD1201-Q1 Other Parts Discussed in Thread: TMP61 , TPLD2001 , TPLD1201 Hi Team,
I would like to see if it would be feasible to utilze the TPLD1201-Q1 as a temperature sensor aggregator with a single altert output.
In this usecase I…
Part Number: TPLD1201-Q1 Tool/software: Hi team,
Does the internal analog comparator have rail-to-rail input or output?
Best regards,
Shunsuke Yamamoto
Hi Juan,
If you're looking for a non-inverting buffer that operates at 5V and accepts 1.8V logic, there are not many single-chip options. You could look at TPLD801-Q1 or TPLD1201-Q1 which can be configured in this way.
Are you able to have the device…
Part Number: CD4027B Other Parts Discussed in Thread: TPLD1201 , TPLD1201-Q1 Tool/software: Hello,
My customer uses automotive qualified JK-FF of OnSemi. They looked through TI web pages, but there is no Q1 devices for JK-FF. They only know OnSemi who…
Hello Albert,
Thank you for your response! To clarify, if I set the reset mode of the counter block to anything besides "High Level Reset" I still get a one period pulse right at the beginning of the simulation. From the description in InterConnect…
Part Number: TPLD1201 Tool/software:
Translator
Hello team
Is there a way to have access to the PAROUT[7:0] bus of a CNT/DLY/FSM block in order to use q0/q1/Q2/.... of the counter ?
Regards
Part Number: TPLD1201 Tool/software: Hi Team,
Please give me your advice on my questions bellow.
Q1. Can you provide me the timing information on the minimum set up (tsup)
and hold (thold)time of flip-flops relative to the clock.
Q2. Can you…