Part Number: TPLD1202 Hi team,
According to section 7.3.13 of the TPLD1202 datasheet, serial communication can be used to update specific registers.
I believe that by rewriting certain registers, it is possible to modify the internal settings of the…
Hi Frantisek,
The TPLD801 and TPLD1201 cannot be programmed without the TI programmer and EVM. TI can provide pre-programmed devices or samples.
However, TPLD1202 and TPLD2001 can be fully programmed without the TI programmer. The details can be found…
Part Number: TPLD1201-DGS-EVM Other Parts Discussed in Thread: TPLD1201 , TPLD1202 Tool/software: Hello TI team,
I am currently trying to supply externally the TPLD1201 through the EVM board with 5V, as this represents the required logic voltage for…
Part Number: TPLD1201 Other Parts Discussed in Thread: TPLD1202 Tool/software: Hello Team,
with the TPLD1201 EVM, it is possible to load the bitstream into the PLD and test it without flashing the OTP. Is it also possible to program the TPLD1202 serially…
Part Number: TPLD1202 Tool/software: Hello TI team, I am currently working with a TPLD1202 EVM module with the Programmer. I am at the stage of making measurements in the laboratory with an oscilloscope for a designed PLD circuit, and I want to supply…
Part Number: TPLD2001-RJY-EVM Other Parts Discussed in Thread: TPLD2001-DGS-EVM , SYSCONFIG , TPLD2001 , TPLD1202 I followed the EVM setup guide in terms of connecting the programmer to the EVM and swithcing on SW0. I have also installed the necessary…
Part Number: AM620-Q1 Other Parts Discussed in Thread: OPT3001 , SK-AM62-LP Hello TI Team,
We are using a custom board based on the AM6204ASGFHIAMCRQ1 with the TPS6521920W RHBRQ1 PMIC and Processor SDK Linux 11.01.05.03 (Yocto) using k3-am62-lp-sk.dts…
Yes, it is. Please help check the log below (the subsequent steps).
Do we need any additional configuration to make sure the system retains the U-Boot setting and boots from the boot partition that we most recently selected?
Step1: Pressed boot mode…
Here is how I compiled DM firmware for SDK 10.0 some time back.
$ pwd /home/lb/sdk/mcu_plus_sdk_am62x_10_00_00_14 $ make -s -C examples/drivers/ipc/ipc_rpmsg_echo_linux/am62x-sk/r5fss0-0_freertos/ti-arm-clang all PROFILE=release $ cd examples/drivers…
Hi Gokul,
I am using the official TI J721S2 EVM , not a custom board.
Other than the device tree changes you provided, I have not made any other modifications to the SDK.
↓ only k3-j721s2-common-proc-board.dtb shows a recent date …