Hi Praveen,
The power supply is about 200cm from the IC, and I add the capacitor close to the vcc pin of TPS24701(parallel with c133, c147(10uF)is the capcitor that I added). When I test the waveform, I added a 30ohm resistor (R458) to GND behind the…
Part Number: TPS2067 Other Parts Discussed in Thread: TPS2066 Is it possible to operate all 3 switches of the TPS2067 in parallel to increase current capability similar to the TPS2066 from this application report? SLVA195
Part Number: TPS2052 Other Parts Discussed in Thread: , TPS2066 , TPS2062 Hi
We are using TPS2052 in one of our design. The continuous load current in datasheet is given as 500mA, can we load this device continuous to 1A.
Hi Bob
Only TPS2066C devices have ESD specifications for Contact and Air.
For example, there is no such specification in the TPS2066.
And TS3USB3000 is QFN, but there is no such specification.
What's the difference?
Thanks
Taemin
Other Parts Discussed in Thread: TPS2066 Hi,
I'm using TPS2054BD in my design for generating 5V USB VBUS voltage.
I'm using this for USB OTG device.
I've a observation, when the board is turned off and OTG cable is connected to board, I see a small…
Other Parts Discussed in Thread: TMS570LS20216 , TPS2066 Hello
In TMS570LS20216 MDK to which peripherals are the GIO pins (A,B) mapped to ? I find GIOA 0,3,4,5 connected to LEDs, GIOB 0,1 connected to TPS2066. Any GIO pin available for toggling or testing…