Part Number: TPS25730 Hello, is it possible to configure the TPS25730 via external resistor ratios into ADCIN3 and ADCIN4 as 0.5A for both min and max current? The datasheet says the min and max can be set to the same current, but table 8-6 does not list…
Part Number: TPS25730A Other Parts Discussed in Thread: TPS25730 is the TPS25730A pin compatible with the TPS25730? what are the functional differences?
Part Number: TPS25730A Other Parts Discussed in Thread: TPS25730
What is the TPS25730A?
The TPS25730A is a stand-alone USB Type-C and Power Delivery controller optimized for applications supporting USB-C PD Power Sink-only applications.
Why…
Part Number: TPS25730 Does the TPS25730DREFR has one or more bytes in the eeprom left, so the user can use them to write some user specific data into the those dedicated registers? If yes, please let me know: - which register - how to access (write/read…
Part Number: TPS25730 How can I clear the Dead Battery flag of the TPS25730 or TPS25730A via I2C? The flag is not mentioned in the reference manual slvucj7.pdf.
Part Number: TPS25730 Hi,
We are designing a Board which is USB Powered. We are using (TPS25730SRSMR) to provide PD Negotation and supply from the external Host.An external 5 V/12 V USB Power Delivery (PD) adapter is connected to the PD sink port.The…
Part Number: TPS25730 Other Parts Discussed in Thread: TPS25751 , , TPS25751A Hi team,
My customer was wondering if there was a way to turn off the PP in the device (PPHV to VBUS) using I2C register settings?
My understanding is that the device does…
Part Number: TPS25730 Other Parts Discussed in Thread: TPS25751 Tool/software: Does TPS25730/25751 have OCP? Or only for RCP? If no OCP, why are there no OCP? Do you have similar device which has OCP?
Part Number: TPS25730 Hello I'm Jaeho
I have a Question, plz check the below
1) When an error occurs on the TPS25730,
Will the PLUG_EVENT PIN status change as well?
Or does it change solely based on cable Connection Present/No Connection Present…
Part Number: TPS25730 Hello I'm Jaeho
I have som Question about PLUG_EVENT
If only VBUS power is applied to the IC and CC1 and CC2 are not connected,
How does PLUG_EVENT Level? ex) High?? or Low??