So I included the pp file And the command line is :
/opt/ti-rtos/am57xx/2.0/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 -O3 --opt_for_speed=5 --include_path="/opt/ti-rtos/am57xx/2.0/ti-cgt-c6000_8.1.3/include" --include_path="/opt/ti-rtos/am57xx/2.0/mathlib_c66x_3_1_1_0…
Part Number: CC1352R Other Parts Discussed in Thread: CC1310 Hi,
My setup:
Sensor
CC1352R custom board
RSSI -47..-52 (image 2)
SDK 3.30.0.03
TI 15.4 stack Linux
3.30.00.12
CC1310 Launchpad as coprocessor with SDK 3.20
I´m sending…
Hi Jonathan, Yes, the values in the datasheet are what is to be followed. WEBENCH is also using the correct pin strap resistor values. Attached is the updated excel calculator tool. The 10kOhm resistor value should result a 400kHz fsw. Recommended for…
Hi Cheryl,
Can you provide more details on where you would like to perform a switch of context?
ARM Architecture.pdf
The attached document from ARM consists of supported instructions which you can refer to and analyze for your use case.
Regards…
Part Number: CC2640R2F Hello,
We have developed firmware using cc2640r2. The cc2640r2 act as slave. Now we want to perform end- Product Tests . Some of the Tests we have done using PTS dongle .
But still the link layer tests are not done.
We want…
Hii,
I tried to perform learning cycle but every time i stuck at the 4th cycle of relaxing battery where battery update status should change to 05 from 04. I am unable to do further procedure from here because update status is not changing to 05 from…
#1: Tell me more. #1-1 What can be the reason why the discharge simulation ends immediately? #1-2 If the Terminate Voltage is set to 3000mV, is it possible that the "normal" FCC will be calculated because the discharge simulation will not end immediately…
5126.spnu515b.pdf
Dear QJ Wang
I wanna watch the TX/RX state,but still have not found the ACK bit in this datasheet”spnu515b”.Could you tell me where to find ACK register bit in the attachment named "spnu515b"? It is better to know which page in this…
Dear Pavel,
Thanks for the above pointers, we are looking into it and modifying u-boot and testing,
I have attached two logs of kernel panics,Kindly provide me feedback for the reason for such a panic, It occurs randomly when system runs for more…