Part Number: INA225-Q1 Other Parts Discussed in Thread: INA225 , CSD Hello Team
We are trying to simulate the spice circuit on PSpice & LtSpice but we are getting some error with library of TPS2H000B
In case of pspice, I have used same simulation profile…
Part Number: TPS2H000-Q1 Hello Team,
My customer have question about internal protection diode.
Do you know which pin has such internal protection diode?
Regards,
Yuta Kurimoto
Part Number: TPS2H000-Q1 We use TPSH000-Q1 (version A)
2-Channel Output Load are LED Module.
Chip support Open Load Detecting function.
But. We don't use open load function because it can't perform certain function.
So. Diag_EN : Disable
…
Part Number: TPS2H000-Q1 Hi,
I am observing unexpected power loss in at TPS2H000A chip. It is around 0,5 Watt and the conditions are following: t(a)=22 deg.C, V(VS)=24,0 Vdc, V(IN1)=V(IN2)=0 V, No load at OUT1, OUT2 (nets VAC_V1, VAC_V2 left open), pull…
Part Number: TPS2H000-Q1 Hi team,
I am using TPS2H000-Q1 (A version) for my current project.
I would like to know the detection time for short-to-ground / short-to-battery.
please let me know.
Regards,
Part Number: TPS2H000-Q1 Hi team,
In some my customer's use case, CH2 is not required. But they don't want to put an external pull down or connect to GND directly to reuse the circuit design.
Is it okay that they left IN2 and SEL floating?
Best…
Part Number: TPS2H000-Q1 Hi Experts,
I want to use TPS2H000-Q1 for a LED driving module.
The module include several LED drivers, LDO and Timer.
When I simulate them on pspice, I can see transient current about 1A~2A when start operation like attached…
Part Number: TPS2H000-Q1 Other Parts Discussed in Thread: TPS1H000-Q1 , Hi team,
My customer is still considering to use TPS1H000-Q1 and TPS2H000-Q1(A version).
They need open load detection in PWM input use case. The PWM frequency is 100Hz to 600Hz and…
Part Number: TPS2H000-Q1 Hello team,
1. What is appropriate current limit range to set for TPS2H000-Q1? Is this 50mA to 900mA as specified in the CL accuracy? Does it mean appropriate R(CL) range should be 4.8kOHm - 267Ohm?
2. The abs max table shows …