Part Number: TPS3850 Hi, Team,
I have a question regarding the WDT function of the TPS3850.
Currently, the TPS3850 is in the following state: WDI = Low SET0 = High and SET1 = Low (WDT disabled)
From this state, SET1 is switched to High (enabling…
Part Number: TPS3850
Hi team,
I have some questions about one of your components that I am currently working with: the TPS3850H50.
For design reasons, I need to add an RC network in front of the Vsense pin (not VDD) to delay the reset signal by…
Part Number: TPS3850 Tool/software: i am using this circuit to monitor the window of , is the design calculation ok? But i have one doubt if i am monitoring 3.3V & both VDD & sense pins are connected to the same, the circuit will be wrong right? If the…
Part Number: TPS3850 Tool/software: Hi, team,
Is [1.05] in equation (15) in the datasheet the correct value? If this value is taken from Table8-5, I assume that [1.095] is the correct value, but am I wrong?
Best regards,
Sato.
Part Number: TPS3850 Tool/software: Hello,
I need to know if TPS3850 is ASIL and can be used for safety applications? if yes can you provide me with safety manual?
Part Number: TPS3850 Other Parts Discussed in Thread: , TMS320F2800157 Tool/software: In a previous thread , I inquired about the ASIL rating of the TPS3850, and the response was as follows: "The TPS3850-Q1 is not an ASIL rated device. However, we do…
Part Number: TPS3850-Q1 Hi, Team
Valeo want to do thermal shock simulation of TPS3850H33QDRCRQ1 .
We need BU support to provide the following information: CTE(coefficient of thermal expansion, young's modulus, and die size.
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 , Hi TI expert
Can you provide your proposals regarding the CCF analysis between voltage monitoring and WWD under the fact that no DFA is available from TI side.
We must demonstrate…