Part Number: TPS3899 Hi experts,
May I know why the td 6.2ms in EC table with CRT cap 10nF is not matching if we apply 10nF to the equ2? Using equ2 with 10nF, the td would be 6.6626ms.
BR,
Allan
Part Number: TPS3899 Other Parts Discussed in Thread: TPS3710 Tool/software: Hi,
I am looking for a replacement for LTC2915HTS8-1#TRMPBF.
I was wondering if you could tell me which products support voltages up to 12V and can set the threshold voltage…
Part Number: TPS3899 Tool/software: Hello Team,
Need quick response for below topic,
I couldn't get a clear answer to the following statements from your feedback,
“In this situation, the SENSE voltage is applied to the IC before reaching the VDD…
Part Number: TPS3899 Tool/software: Hi TI team,
I have recently completed validation of the circuit using the TLV840MADL13DBVR, and it is working correctly. I want to reduce the PCB area. Therefore, I plan to replace the TLV840MADL13DBVR with the…
Part Number: TPS3899 Other Parts Discussed in Thread: , TPS3842 Hi
I am caculate the range of the tD-SENSE (min) or tD (min) and the tD-SENSE (max) or tD (max) .
I can not find the Rct(min) Rct(max) and tD(no cap,min) in the datasheet.
Only typical…
Part Number: TPS3899 Other Parts Discussed in Thread: TPS3851 dears,
My customer is seeking for 20s and 50s delay watch dog, i'd like to recommend TPS3899 for lowest cost, but according to the datasheet, the max delay time is 6.2S with 10uF capacitor…
Part Number: TPS3899 Tool/software: Hello,
I am looking to find information if TI can supply military device.
The temperature range -55C to 125 degree C.
thank you,
Part Number: TPS3899 Actually we are planning to used this part in our one of the design but the issue is this actual part having the pitch different as compared to the pcb footprint recommendation due to which the components leads not sit properly on…
Part Number: TPS3899 Other Parts Discussed in Thread: TPS3422 , TPS3808E , Hi
Customers reported that the TPS3899DL30DSER board cannot be turned on after calling it back, and RST# has no effect. Can you help identify the problem? Thanks