Part Number: TPS54060A Other Parts Discussed in Thread: TPS54060EVM-590 , We use this device for a +/-15V power supply, similar to the TPS54060EVM-590, nominal input voltage 24V.
We are using the TPS54060A for several years now. We received a new batch…
The evm and app note may work for you. It generates a +/- output from a 24V input, but it also can work down at 5V.
Split Rail EVM
http://www.ti.com/tool/tps54060evm-590
Split Rail App note
http://www.ti.com/tool/swiftposneg-calc
Kyle,
If you have not found this material on the TI website, you may find this helpful
Excel Sheet
Positive and Negative Output Voltage Split Rail Calculator for SWIFT DC/DC Converters
http://www.ti.com/tool/swiftposneg-calc
Reference…
There are two choices
Create an Inverting Power Supply from a Step-Down Regulator
http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=slva317a
Excel Calculator for the above appnote http://focus.ti.com/docs/toolsw/folders…
Rob,
It looks like what you really need is a DC/DC converter because the TL7660 is only a solution for low power and low voltage conversion. The link posted below is one of the two parts that meets the requirements of +14V in and -14V out at 100mA…
Other Parts Discussed in Thread: TPS54060EVM-590 , TPS63700 , TPS54060 As mentioned in my post to this forum "SLVA369 circuit in TPS54060EVM-590 positive output not equal to negative?" I am perfecting a power supply subsystem using Vin of 4.5 to 25 VDC…