Part Number: TPS54062 We use TPS54062 for more than 10 years to create 5V for the control circuit of a lamp driver we obseved disturbances of the TPS54062 bucker to the main switch mode LED lamp driver. There is High Noise level which is expressed in…
Part Number: TPS54062 Hi team
What will happened when it is over load? My customer's application is Vin 35V and Vout 5V. And they are wondering what happened when Iout is over 0.05A.
I see frequency foldback in this situation. If so, could you give…
Part Number: XTR116 Other Parts Discussed in Thread: XTR117 , TPS54062 Tool/software: Hello,
I changed my design to the following:
The problem now is that the switch output is ~68mA instead of 20mA and C11 burns through. Could it be that the…
Part Number: TPS54062 Tool/software: Hi,
I am trying to design a constant current source output using TPS54062 (or any other low IQ buck convertor) to drive a coil using an H-bridge.
1) Vin = 24V.
2) Vout < 0.5V.
3) Output Current = 25mA max …
Part Number: XTR116 Other Parts Discussed in Thread: TPS54062 , XTR111 My circuit diagram shows a 4-20mA transmitter with the XTR116 and TPS54062. Instead of 4mA I get 34mA.What could be the reason for this?
Part Number: XTR116 Other Parts Discussed in Thread: ISO7310C , XTR110 , XTR111
My update.
I connect the Loop GND to the 2 pin connector (+24V and GND) and then I let the Float_gnd (only pin 3 from the XTR116) "float" on the PCB, with out connection…
Part Number: TPS54062 hello
I am trying to do a 50mA 2S nimh batterie charger using the TPS54062
i have input voltage of 12VDC, output voltage set to 3
while using the TPS54062EVM, the current limits was triggered at 90mA ( Iout), i prefet to limit…
Part Number: TPS54062 Hi Experts,
Customer is using the TPS54062 in a product to convert 24v to 3.3v. During the assembly (after testing and programming), we will also have to configure the microcontrollers on this device. To do this, they need 3.3v…
Part Number: TPS54062 We use TPS54062 for 5V auxiiary power supply In our schematic the enabe pin is open We suspect 5V voltage drops following transmitted interference to our product Question: can we place a 10nF to 100nF capacitor at the enable input…
Part Number: TPS54062 hello.
I designed a board with a power input of 40V to 60V and an output of 6V using the TPS54062 with reference to the circuit diagram above.
When 40V is applied to this board, 6V output comes out properly.
However, when 55V…