Part Number: TPS54360B Hi Teams,
The schematic above is for robot applications, where the input is 24V to 5V to supply power to the onboard system and magnetic encoder. Please help to check if there are any issues.Thank you!
Part Number: TPS54360B-Q1 Other Parts Discussed in Thread: TPS54360B Hi,
I am using the TPS54360B-Q1 in my design to generate a 12 V, 3.5 A output.
Input voltage range: 8 V to 60 V
I am able to obtain a stable 12 V output under no-load conditions;…
Part Number: TPS54360B hi expert
I am designing a power supply using TPS54360B with a maximum input of 50V and an output of 15V/1A.At present, it keeps exploding when in use. It seems that the internal MOS transistor has blown up.Currently, it keeps…
Part Number: TPS54360B-Q1 Hi team,
Could you share functional safety FIT, pin FMA document with me? My customer is doing FuSa analysis for their system. We have valid NDA with them.
You can share with me via email.
Ethan Wen
Part Number: TPS54360B Dear TI Quality Support Team,
I am writing to report a quality issue discovered during our incoming inspection of TI components, which were sourced through Arrow Electronics.
We performed 100% X-ray inspection on multiple reels…
Part Number: TPS54360B Tool/software: hi,
The customer is using TPS54360B for an output voltage of -15V, an output current of around 0.5A, and an input voltage of 24V. Please help review the schematic diagram. Thank you!
Part Number: TPS54360B Other Parts Discussed in Thread: TPS54360 , LM70840 I assembled a circuit based on a WEBENCH design using the TPS54360 for a 5–54 VDC input and 3 A output. However, when I power the circuit with 54 VDC, it burns out as soon as I…
Part Number: TPS54360B-Q1 Other Parts Discussed in Thread: TPS54360 Hello, We are currently using TPS54360B-Q1 regulator and TAS5760MTDAPRQ1 amplifier. Due to sudden in-rush current, the regulator is not able to power up amplifier properly. Can you please…
Part Number: TPS54335-1A Other Parts Discussed in Thread: TPS54360B , Tool/software: Hi team,
Regarding toTPS54335-1A and TPS54360B,
Could you please let us know at what multiple (or percentage) of the Vout the OVP is triggered? Best regards, Got…