Part Number: TPS61322 Other Parts Discussed in Thread: TPS61299 Tool/software: I hope this message finds you well. My name is Chandrakant Pardeshi, and I am writing on behalf of M-Tech Innovations, Pune. One of my colleagues, Smarudhi Sakhare, recently…
Part Number: TPS61322
Dear friends,
We have integrated the TPS613221A as the input regulator in the design of our battery-powered device. We used the reference circuit from the datasheet, where the ZLLS410TA diode is recommended as D1.
The circuit…
Part Number: TPS61322 Other Parts Discussed in Thread: LM5123-Q1 , TPS61299 Dear Team,
My customer is designing the application circuit of the TPS61322A, and they would like to desing the application circuit so that they can measure the phase and gain…
Part Number: TPS61322 Other Parts Discussed in Thread: TPS61099 , TPS61299 Tool/software: We tried to boost the voltage up to 3.5 V from 1.2 V. But the voltage is not increasing . Please help us with its circuit diagram.
Part Number: TPS61322 Other Parts Discussed in Thread: TPS61099 Tool/software: What is the I_IH for TPS61322?
We are looking for this in regards to the enable pin.
Thanks!
Part Number: TPS61322 Tool/software: Hi team,
Customer use TPS613221A to get 3.3V in their design, They follow EVM design, could you help check following design?
Vin max 2.5V.
Does 4.7uH the most recommend inductor?
Regards,
Will
Part Number: TPS61322 Tool/software: Hi,
I plan to use the TPS613222A to get an output voltage of exactly 5V. The input is USB, so it can be in range 4,4V..5,25V.
So what I do not understand from the data sheet: it specifies the output voltage range…
Part Number: TPS61322 Other Parts Discussed in Thread: TRF7970A , , TPS61299 Tool/software: I have a circuit with a 3.7V LC26650 battery feeding a booster TPS613222ADBVR to get an output of 5V. I have tested the circuit in the picture below with and without…
Part Number: TPS61322 Other Parts Discussed in Thread: TPS61299 Tool/software: Hello TI experts!
I am trying to select a switching Regulator for my company's design where PCB is very small. I have evaluated many regulators, and read many articles on…
Part Number: TPS61322 Tool/software: Dear TI team, using the proposed circuit (Power Designer) for the TPS61322 (1.8 to 3.6 V input voltage, 5 V output voltage @ 0.1A) we experience a high inrush current (~0.8 A) when turning on the device using a high…