Part Number: TPS62441-Q1 As specified in Section 9.4.2 of the datasheet, the mode switching threshold is approximately 0.8 A. Each channel of TPS62441-Q1 has a full-load current of 1 A. We would also reserve sufficient margin in design, so the maximum…
Part Number: TPS62441-Q1 Other Parts Discussed in Thread: TPS62441 Hello everyone!
Could you please explain how to calculate the output ripple of TPS62441 in PFM mode?
Thank you.
Part Number: TPS62441 Other Parts Discussed in Thread: TPS62840 , TPS62843 Hi team,
My customer is searching for a dual output buck converter for smart watch application, output 1 0.75V/100mA; output 2 0.85V /100mA.
I find TPS62441, it's dual output…
Part Number: TPS62441-Q1 /resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/pastedimage1707125579790v1.png
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/pastedimage1707125695939v1…
Part Number: TPS62441 Tool/software: Dear Support Team,
As part of a reliability analysis based on the VITA 51.1 standard, we are currently collecting failure rate data for components used in our systems.
Could you please provide the following…
Part Number: TPS650250 Other Parts Discussed in Thread: TPS62441-Q1 , TPS6521905 , TPS6593-Q1 Tool/software:
Application detail:
We are looking for a Power Management Integrated Circuit (PMIC) that can provide 3.3V, 1.8V, and 0.9V outputs. This PMIC…
Part Number: TPS62441-Q1 Tool/software: Hi team,
We would like to inquire about short circuit test using an e-load set to 0.05 ohm in CR mode.
The waveform is as shown below.
Could you please help check if the behavior is correct and explain it…
Part Number: TPS62441-Q1 Tool/software: Hi, I need TPS62441-Q1 PWM rising, falling time because of EMI simulation. we operate 2.2Mhz
if TI don't have rising, falling time spec, please give me a measuring value.
our company use this product and we…
Part Number: TPS62441 Dear e2e,
I would like to use TPS62441, its a great part. I need to synchronize its switching frequency to exactly 2MHz by applying a external clock to the SYNC pin.
I can see from the datasheet 7.5 and 7.6 these specifications…
Part Number: TPS62441-Q1 Tool/software: If I were to set the switching frequency at 4 MHz and have the compensation set for smallest output capacitance with SSC enabled, I calculated Rcf using Equation 2 as seen in the image below:
The Rcf result…