Dear TI:
I added the log to print "img" from function "forward"( /edgeai-mmdetection/mmdet/models/detectors/base.py ):
def forward(self, img, img_metas, return_loss=True, **kwargs):
"""Calls either :func:`forward_train`…
Hi sir,
The above issue is due to the consideration of width instead of stride while reading the output image of our custom node. The issue is resolved. The application is running now. But after running the app for 2 or 3 minutes, the following log is…
Hello Moritz,
I apologize, missed your question in my first response
1. Is there any major difference between the two chip versions? I am afraid the ACT/SLEEP - Edge Triggered might cause the issue ?
You are correct one is level triggered and one is edge…
Hi,
You are right, my battery is 2S1P. After changing it to 2, I obtained the correct report from the GPCRA0 tool feedback. Please review the report content. I imported the gg_out.csv file of the report and conducted a charge and discharge test. Are there…
Hi Pratik Kedar, I found that the problem was at C7x_1. [C7x_1 ] 412.410605 s: VX_ZONE_INFO:[ownTargetKernelExecute:398] Done executing process callback for kernel [com.ti.tidl] [C7x_1 ] 412.410640 s: VX_ZONE_INFO:[ownTargetNodeDescNodeExecute:683] Node…
Hi Alvaro,
sorry for the late response. It is not easy to communicate and manage the test with our customer. I got the new register dump now but with the custom switch set 100M full duplex, negotiation off. We also test your sk-am62 develop kit ( SK-AM62…
I am 99% sure there are no conflicts (I used the sysconfig program to get the initial DT), I have looked @ the pin mux registers, and they look to be in a sane state for the 2 I am most focused on at this point,
Here is the debug FS file of the pin mux…