I created a circuit with reference to TUSB8020BPHPEVM Schematic,
but it does not work. Ask if you need to put binaries in eeprom or just usb hub operation through dip sw control.
sllu196.pdf Also ask the eeprom programmer file
Hi:
I am a Enrique´s colleague.
Our device is an endpoint device that makes CPSW work in dual mac mode and ony have one ethernet interface port.
Attached is the "ifconfig -a" command output.
Attached is also the device´s dts and we are using the…
Part Number: AM5706 Other Parts Discussed in Thread: TPS22965 , TPS51200
Hi Team,
My customer is planning to evaluate our AM5706. Schematic is on-going now and here comes two questions from customer, need you kindly check, thanks!
Below is the reference…
I'm sorry, here below you can find the screen shot and the schematic.
I'm preparing a sketch with the architecture of the I2C paths.
Thanks a lot.
Best regards Edo.
621_20_0176_03.pdf
Jeff,
I am not familiar with the capabilities of the TDA4 EVM. Also maybe you can just remove the 960 unit off the EVM and put it onto the TDA4 EVM.
Brijesh Jadav
Brijesh,
Do you know if we connect the 960 EVM to the TDA4 EVM?
snlu226b.pdf…
Dear SJ -
Thanks for the post and welcome to E2E!
Sorry for your issue - here is looks like the MOSFET Q2 (CSD18543) had an issue.
Since that it is after the reverse polarity protection (Q1 of same kind of device, see attached schematic), I would…
Part Number: AM5708 Hi:
I have a AM5708 custom board with SDK5.02. I have implemented PTP over GMAC and am using timer13 for PPS output.
I have just moved to SDK6.02 and have realized that timer13 is not properly initialized by Linux, in fact I have…
Part Number: AM5708 Other Parts Discussed in Thread: DRA718 , DRA72 , DRA722 , PCF8575 , TLV320AIC3106 , LP8733 , TPD12S015 , CSD Tool/software: Linux Hi: I have a custom AM5708 based board and SDK Linux 05.00.00.15. Attached are the device tree and defconfig…
Hello ABUBHAV
When I removed the SD card, the board powers ON for about 5 seconds and powers OFF. I tried setting jumpers based on the document below but it did not work
AM572x General-Purpose EVM Hardware User's Guide.pdf
516582e_vayu_evm_28aug_2013a.pdf Tsvetolin Shulev,
I have tried as you suggested.
Now the "mmc0: host does not support reading read-only switch, assuming write-enable" message is coming" after the below modification in DTS File.But still the File…