Part Number: TPS82085 "Regarding part number TPS82085SILR in the package outline ( SIL0008C ), a maximum height of 1.33 mm is mentioned. It seems this might be without the lead plating thickness. What is the expected overall height from the PCB surface…
Part Number: TPS82085 Dear TI Support,
I am currently using the TPS82085SILT DC/DC converter to generate a 1.8 V output from a 3.3 V input supply (maximum input voltage of 3.63 V).
When I apply a 100 mA load to the 1.8 V output, I measure an efficiency…
Part Number: TPS82085 Tool/software: Hi Engineer,
I purchased the part of TPS82085SILR, and there is no marking on the top side and back side.
Could you help check whether the part are correct?
Thanks,
Suri
Part Number: TPS82085 hi,
The design schematic diagram of TPS82085 is shown below. Could you please help check if there are any issues? Or good advice?
Part Number: TPS82085 Other Parts Discussed in Thread: TPS62085 , Hello,
Does the TPS82085 use the same die as the TPS62085?
Best regards,
Denis GALLARDO
Part Number: TPS82085 Other Parts Discussed in Thread: TPS82084 Tool/software: Dear Team,
our customer is using the power module TPS82084 for 6V Vin step down rail.
however due to some defects of the PCB silk ink, their factory production line…
Part Number: TPS82085 Tool/software: Hello,
Could you please tell us what type of inductor is used in TPS82085?
For example, is it an inductor type like the one below?
Thank you.
JH