Hi Mariano,
This EVM was designed using PADS software and not Altium/Protel so the original documents may not be very useful for you. It looks like the output port of the TPS84250 is accessible. I recommending ordering the TPS7A4700 EVM (where the output…
Other Parts Discussed in Thread: PMP8372 , TPS84250 , TPS84259 Hello,
i'm looking for an EVM with a DC input that must be capable to deliver ±12Vdc with PSRR ~100dB in 0-3Khz bandwidth.
I've seen PMP8372 module and it would be perfect but i…
Other Parts Discussed in Thread: TPS84250 , PMP8372 Hello,
I see that there are individual evaluation modules for the TPS84250 and TPS7A4700, but for my application having the physical PMP8372 reference design would be more beneficial.
I do see that the gerber…
Oh guys pardon me,
I found the document I was looking for in another post:
TPS84250 and TPS84259 land/pad Dimensions
Thanks to moderator because moving post I saw it immediately.
Best regards.
Luca
PTN series was introduced 8 years ago. This is a very popular module. There is no life time data on presently manufactured products.
TI recently released TPS84250 which has the same voltage ranges with up to 2.5A load with internal inductor.
Tom
Other Parts Discussed in Thread: TPS84210 , TPS84610 , TPS84250 Pls tell me package size as below devices.
1.TPS84210
2.TPS84610
3.TPS84150
Best Regards, MRB Sasaki.