Part Number: TRF3765 Hi everyone,
I am using TRF3765 PLL in my design for generating 3200MHz output from 25MHz reference clock.
Loop Filter used in my design is almost same as the design in data sheet for fpd of 1.6MHz.
C1 = 47pF, C2= 560pF, R2= 10Kohm…
Part Number: TRF3765 Hi,
We are using the TRF3765 as an RF LO in the 2-4 GHz range, with a 10 MHz external reference.
At room temperature we have no issues, but at ~5 C the chip fails to lock detect when programmed with a new frequency.
Any ideas on what…
Part Number: TSW3065EVM Other Parts Discussed in Thread: TRF3765 , LMX2594EVM , LMX2594 , LMX2592 , USB2ANY , LMX2592EVM Tool/software: Dear TI,
We have 2 inquiries regarding TI PLLs:
First inquiry
We have acquired a module, the TSW3065EVM, which generates…
Part Number: TRF3765 HI,
I just bought the TRF3765 EVAL BOARD FROM DIGIKEY and there is no CD in the box.
So I need the GUI SOFTWARE but I can't find the page on ti website to download it.
Someone can help me ?
Best regard,
Part Number: TRF3765 Other Parts Discussed in Thread: LMK61E07 Greetings,
I am in need for a synthesizer that can output 900 MHz sine wave. Is there a part you can help recommend?
The PLL needs to be one time programmable (OTP) so that once power reset…
Part Number: TRF3765 Other Parts Discussed in Thread: LMK04828 , ADC12J4000 Hello,
I am using ADC12J400 EVM. This evm uses TRF3765 for clock generation.
For automation, I would like to program TRF3765 using a little c program that I have created. C program…
Part Number: TRF3765 Hi all,
My customer plans to use TRF3765. Could you please tell me the recommended value of fPDF, NINT, NFRAC and etc. for minimizing the phase noise and the spurs under the below conditions?
VCO frequency: 3720MHz - 3780MHz
Channel…
Other Parts Discussed in Thread: TRF3765 Hi,
Would you please tell me if the 4 outputs of TRF3765 are phase aligned after the pll locked?
Thanks a lot.
Parker
+8610 13811174507
strongfei@163.com