Part Number: TRF37A73 Hi,
My customer uses this device in the range 917-921MHz, can I get S-parameters for this frequency band?
Thank you for your support.
Hiroshi
Part Number: TRF37A73 Other Parts Discussed in Thread: TINA-TI Hi,
Our customer inquired about "variation in gain with temperature of the TRF37A73IDSGR". The temperature range is -20°C to 60°C. Customer says it's OK to use simulation instead…
Part Number: TRF37A73 Hi,
Q. Could you tell me the resistance value and tolerance of the internal pull-down resistor on the PWDN pin?
An NPN transistor is connected externally to switch between Hi and Lo. However, the current design is 1.95V at Hi.
The…
Part Number: TRF37A73 Hello, stated that TRF37A73 is operating well below compression, which is the difference in output power in dB between device normally operating (PWDN low) and muted (PWDN high)?
Part Number: TRF37A73 Other Parts Discussed in Thread: TRF37D73 , Hi gents,
I've got 2 questions related to the TRF37D73 :
- I would like to increase output power of a DECT module, this module got a maximum RF output of 23dbm ( according to regulation…
Part Number: TRF37A73 Hi Team, We have a customer inquiry regarding designing with TRF37A73. Our customer would like to ask for guidelines for how to cascade successfully two parts of TRF37A73 in order to achieve a broad-band response over the entire component…
Part Number: TRF37A73 Other Parts Discussed in Thread: TRF37B73 Hi team,
Could you please help me pick up Broadcom alternative?
Part#:MGA-62563-TR1G
Requirement:
- frequency:approx. 50MHz~450MHz
- GAIN:approx. 22dB
- Input voltage:5V or 3.3V
- NF:< approx…
Part Number: TRF37A73 From the datasheet, the absolute maximum input power for this device is +10 dBm. This seems very low for most gain blocks and LNAs. Usually the number is on the order of +20 dBm. Is it possible to have this device see greater than…
Part Number: TRF37A73 Other Parts Discussed in Thread: OPA694 , BUF602 , LMH5401 , LMH3401 , , LMH6559 TRF37A73 output choke is not possible across the frequency range needed. Is there a different part that is better suited to this application?