Part Number: TRF37B73 Hi TI
I am facing problem, that the input return loss S11, is very depending on the input power level and output load. As well I get rippel in the gain (S21), as function of input power level and output load. The input power level…
Part Number: TRF37B73 Hello team,
I have a quick question.
Can +10dBm as input power absolute max rating be applied to when the device is in power down state?
Best regards,
Part Number: THS9000 Other Parts Discussed in Thread: TRF37C73 , TRF37B73 , TRF37A73 Hello,
We have recently tested your eval-board for THS9000, and the IC seems to fulfill our requirements regarding its performance.
However, it is stated on you home…
John, have you looked at the TRF37B73 RF amplifier. it is much newer than the THS9000. Operates at 3V3, 52 mA, no bias resistor vs the THS9000 3V ~70 mA with a 100 ohm bias.
Also a little lower cost.
Hello Ed;
thank you very much for the fast response.
We are using TI: TRF37A73, TRF37B73, TRF37C73 amplifiers and this application that I'm working on, is a RF matrix with 4.25 GHz to 5.5 GHz range and we are going to use TRF37A73 amplifier and I…
Part Number: TRF37A75 Other Parts Discussed in Thread: TRF37B73 Hello,
Our customer is using the TRF37A75 and TRF37B73 devices in their system and they are testing their prototype. The following concern was raised
"
I am currently designing a number…
Part Number: TRF37D73 Other Parts Discussed in Thread: AFE7900EVM , , TRF1208 , AFE7900 , TRF37A73 , TRF37B73 Hello support Team,
I am looking for the RF gain block which is having the internal fast bypass switching for Direct sampling transceiver …
Other Parts Discussed in Thread: TRF37B73 Some my clients are using NXP BGU8007 or MAXIM MAX2640 now for car GPS trackers. I want to replace it by TRF37B73 or similar. But TRF has lower gain, higher noise and current consumption is higher in 6-15 times…
Part Number: TRF37A75 Other Parts Discussed in Thread: LMX2594 , , TRF37B75 , TRF37B73 , TRF37C73 , TRF37C75 , TRF37D73 , TINA-TI Hello:
I'm working a low noise synthesizer development using the LMX2594 fully integrated synthesizer, and the LM2490 with…