Part Number: MAX3243 Other Parts Discussed in Thread: TRS3243 , , TRS3243E , Hi Sir,
What are the differences among MAX3243, MAX3243E, TRS3243 and TRS3243E? Thanks!
Best regards,
Sam Ting
Other Parts Discussed in Thread: MAX3243 , TRS3243 Hello,
Do we have Resistance of Rout of MAX3243 and TRS3243 to provide this specification to customer? Thank you.
BR
Patrick
Other Parts Discussed in Thread: MAX3243 , TRS3243 Hello,
Below is customer issue. Has any comments for clarify? Thank you.
"Below is our block diagram of COM ports, both MAX3243 are from same COM controller (BMC), and Rout are tied togethe…
Part Number: TRS213 Other Parts Discussed in Thread: MAX213 , MAX3243E , TRS3243E , TRS3243 , MAX3243 Hi Expert,
May I know the difference between MAX3243EIDBR & TRS213IDBR?
Which one has the better ESD protection?
BR,
Aaron Chen
Part Number: TRS3243E Other Parts Discussed in Thread: TRS3243 , MAX3243 , , MAX3243E Hello team,
Our customer is planning to replace MAX3243EIDBR for delivery issue, and assumed if TRS3243EIDBR could be considered as an alternative.
In the other E2E thread…
There is no difference between MAX3243 and TRS3243 devices.
The TRS F device supports a higher data rate.
RS-232 and RS-485/422 are completely different, electrically. If you want to support both, use separate transceivers.
Matteo,
As Clemens said, the main alternatives are not available in the same package, however, the TRS3243 does have a VQFN package and has some stock available on TI.com. Would this work for your application?
Regards,
Eric Hackett
Part Number: CD40106B Other Parts Discussed in Thread: TRS3243 , GD75232 , CD4010B Hello,
I have a motherboard that may be connected to an external peripheral, using several signals to communicate between them (UART + controls). The peripheral may draw…
Part Number: TRS3243E Other Parts Discussed in Thread: TRS3243 Hi Sirs, With 3.3V power supply, my customer got signal distortion problem with the TRS3243ECDBR device as the waveforms below: Input Signal (RX before TRS3243) Input Signal (TX before TRS3243…