Part Number: BEAGLE-3P-BBONE-AI Other Parts Discussed in Thread: AM5729
Hi, this is really kicking my butt! I need to get an understanding of the RPMsg methods for the AM5729, all the examples and labs are based on the AM355x processor, which has a…
Part Number: PHYTC-3P-PHYCORE-AM57X hi,
why am I seeing a backtrace dump when calling clGetPlatformIDs(1, &platform_id, &ret_num_platforms)? Backtrace, makefile, and code up to call provided below.
[ 66.404567] WARNING: CPU: 0 PID: 0 at /opt/PHYTEC_BSPs…
Part Number: AM6442
If you are interested in learning more about the new AM6442 Sitara Processor family and the Software Development flows that are used for a successful design, this is a great opportunity. This is the next webinar in our monthly webinar…
Hi Ming,
Thanks for your instructions.
I finished all the above tests just now.
1) Change from debug build to release build indeed increase the CS rate from 69.54 KHz to 91.14 KHz. It's really helpful.
2) Once I enabled DMA as shown in the below…
Hello Andrew,
I'm sure you mean EtherCAT slave here. Technically, it is viable to run Linux and EtherCAT slave on ICE platform. The challenge would be support from TI for this configuration. We were using Linux for Profibus slave solution on AM1810…
Hi Cary, I'm attaching AM62x boot flow slide for your reference, where boot process is similar on AM62x/AM62A. On K3 SoC (i.e. AM62A, AM62x, AM64x...), u-boot/Linux boot is a multi-stage boot process across multiple cores, which makes loading/debugging…
Hi Nadav I see several questions in this thread, so let me see if I can help provide some guidance on them I will start off with saying that the following link is a good "map" to what is our story on the various development platforms and what TI provided…
Hi Divyaa,
Couple comments to help in your seleciton:
AM243x max clock speed is 800MHz but there are multiple core options
AM243x does not supoprt SGMII, but does supoprt RGMII
There are leaded pacakge options.
Please see attached background…
Hi Ya Lin,
This seems to be an issue with your IPU-1 application. I would suggest placing a while(1) loop in the entry point of your IPU-1 firmware (maybe in the main function in MainIPU1.c) and then step through the code using CCS with the JTAG connected…
Hi,
Please see attached details on the AM243x with PROFINET support. Do you have local sales support?
AM243x Device option "F" incudes TI software supporting PROFINET.
2134.AM243x_Overview.pdf
Best regards,
Mike