Part Number: TXS0108E Hi Support team
We have application apply the TXS0108E for SPI leavel shifter, it already built hundrand boards without problem, recently we got problem on it.
The circuit as below, the host is Marvell/OcteonTX2 with 1.8V SPI output…
Other Parts Discussed in Thread: TS3A24157 For I2C switch applications requiring a logic control signal instead of an I2C command to multiplex between two I2C Masters, A and B, the TS3A24157 can be used as a solution to this problem.
The TS3A24157 has…
Hi Kyle,
We do not have an IBIS mode available for the TS3A5223, however, we have one for a very similar device with the TS3A24157 . These should perform very closely within the simulation.
Thanks!
Bryan
Other Parts Discussed in Thread: TS3A24157 I have a project where I use an ARM7 to communicate with CAN via the SN65HVD232D. I would like to add one more CAN channel than the microcontroller supports. I have thought about "multiplexing" the signal, with…
Part Number: SN74CBTLV3257 Other Parts Discussed in Thread: TS3A24157 , TMUX1574 , , TS3A5223 , SN3257-Q1 Hi team,
My customer is looking for a Bus switch.
Requirement
-Switch type : SPDT
-Number of channels : 4bit or 2bit*2
-Power supply : 3.3V for both…
Part Number: TS3A24159 Other Parts Discussed in Thread: TS3A24157 HI All
There is no VSSOP(DGS) package outline information on the datesheet of TS3A24159.
But there is VSSOP package information(Page24) on TS3A24157.
Do they have the same size?
HI Hao,
The CL of 50pF is quite small capacitance - you can use a smaller cap but it will not have a significant effect on the output.
Can you explain how you are using the switch and why you are interested in the THD spec?
Take a look at TS3A24157 . It…
Part Number: TS5A3159 Other Parts Discussed in Thread: TS5A12301E , TS3A24157 Hello,
my customer looking for SPDT device that can provide up to 300mA. He used TS5A3159DBVR in the past, but unfortunately it can't support that current.
For the prototype…
Part Number: SN74HC4066 Other Parts Discussed in Thread: TS3A24157 , TCA9543A
Hi
Let me consider SN74HC4066 as use for I2C signal switching as follows.
What is the issue that would be supposed?
I believe we can offer the better solution if we use…
Frank,
I typed in baud rate in to the switches and multiplexers e2e forum search bar and found this post that should help you with your question.
Use of TS3A24157 for UART switching
Also you can look at the switches and multiplexers frequently asked…