Sachin,
The TS3DS26227 is a unbuffered passive FET switch capable of passing differential up to 800MHz. The device can pass a signal with a 5pF load capacitance as the timing specs in the datasheet were taken with 35pF loads.
Yes, the parasitic capacitance…
Other Parts Discussed in Thread: TS3DS26227 I have a need to switch between an LVDS (differential voltage of 600 mv with common mode of 600 mv) signal and a CMOS signal level of 3.3 V. The switching signal ideally is 2.5 V but I can make it what ever it…
Hello Sepeedah, What's the end product here? You're correct in your assessment that there are no P2P drop in replacements for the TS3A5223. To shed further light on the bandwidth behavior, these devices bandwidths are spec'ed at given conditions…
Part Number: TS3L110 Other Parts Discussed in Thread: TS3DS26227 , TMUX136 , TS3DV642 Dear Support Team,
for a telematic box, my customer needs to switch between 2 connectors towards the same Auto ETH Phy. Q1 qualification not mandatory, aftermarket application…
Part Number: TS3USB30 Other Parts Discussed in Thread: TS3DS26227
Hello Team
My Customer will use TS3USB30 as Clock Switch. Some questions are as follow:
1) Do you have detail information about Vih/ ViL, Voh/Vol, tPH/tPLH
2) Does TS3USB30 be used as Clock…
Antony,
Yes, the TS3DS26227 device can support 720MHz and it is a 2 channel 1:2 mux.
You can also look at the several USB switches that are high bandwidth 2 channel 1:2 mux like the TS3USB3000, TS3USB221, TS3USB30E.
Thank you,
Adam
Other Parts Discussed in Thread: TS5A23157 , TS3DS26227 , CD4052B , TS3A5018 Hi,
I need a 2:1 and 2:1 function as below shows.
I'm looking at analog switch TS5A23157 and TS3DS26227. The system spec are,
1. MUX 100M and 25M data rate from optical module…
Other Parts Discussed in Thread: TS3DS26227 Hi All,
In my design, I have to route some analog differential signals come out of a sensor to ADC and DAC through an analog switch. I have selected TS3DS26227 (SPDTx2) switch for the same. So the signals first…
Other Parts Discussed in Thread: TS3DS26227 , TS3V712E Hello,
I'm looking to multiplex two LVDS signals down to one. The data rate is 680 Mbps DDR, or 340 MHz.
Actually, I'm doing that for a bus 6 lanes wide, so I'm looking to multiplex 12 LVDS signals…