Luke,
What is the voltage level and bandwidth of the differential signal? What is going to be connected to each side of the switch?
The TS5A21366 will work if the signals are within the recommended operating conditions.
If you have a high speed…
Hi,
thanks for you support.
We just defined the power supply of the entire signal chain and "unfortunately" it is 5.0V.
Nevertheless on the datasheet of the TS3USB31E the Vcc Absolute maximum rating is 7V and the "recommended conditions are…
Other Parts Discussed in Thread: TS3USB31 I need a switch for USB D+ D- as below: when lose power it should be high impedance (>1MΩ).
In 1:1 SPST for USB, I found TS3USB31(E), but it is disconnect only when control pin in logic "High", could you…
Atul,
We have several switches in our portfolio that place the signal path in a high impedance state when there is 0V on the power supply. We are currently working on a better way to search for these types of products but the best way to do it today is…
Hello Aaron,
The best solution would be to use a USB switch like the TS3USB221 or the TS3USB31 and also use the switch enable signal to drive the TUSB2036's reset.
I need to check on the lab how are the outputs of the TUSB2036 when its inputs are…
Other Parts Discussed in Thread: TS3USB30 , TS3USB221 , TS3USB31 , TS5N412 , HD3SS3412 Hello,
I'm looking for a USB3.0 switch 1:1 or 1:2 (multiplexer / demultiplexer). In other words, I'm looking for a USB3.0 compliant chip that is equivalent to the TS3USB221…
Other Parts Discussed in Thread: TS3USB30 , TS3USB31 Hi
Found IBIS model for TS3USB31, but need the model of the TS3USB30, can someone poiint me in the right direction or can they use the 31 model and just modify it?
Thanks
Jeffc
Other Parts Discussed in Thread: PCA9306 , TCA9617B , TCA9517 E2E community,
It is common question to ask will (this device) support ( this signal type/standard). When selecting an appropriate signal switch for your signal type/standard you need to consider…