The TS3USB3200 device can support the 480Mbps USB 2.0 data rates required by the USB 2.0 On-The-Go (OTG) specification. You can see below that the device doesn't have much effect on the signal through the MHL path even at 700Mbps which is more than enough…
Hideto,
[Q1] Is TS3USB3200 available with MHL SINK apparatus?
The TS3USB3200 devices is an unbuffered pass FET so it will not sink current through the singal path but rather pass it from the input to the output.
【Q2】 Does TS3USB3200 perform Pulse…
Other Parts Discussed in Thread: TS3USB3200 , TS3USB3000 Hi,
Can TS3USB3000 and TS3USB3200 pass compliance test?
Now, it is usually used for Tx.
Can they pass compliance test in case of Rx as well?
Thanks in advance.
The datasheet specifies that there is a clamping diode for when the I/O voltage goes below ground but not when it goes high. Is this behavior defined? Does it clamp to some level above ground or does the switch FET avalanche causing current to flow into…
Other Parts Discussed in Thread: TS3USB3200 , TS3DV642 Hi Team!
I had a question regarding the TS3USB3200.
Has this been tested to carry HDMI TMDS signals?
Thanks,
Ben
Other Parts Discussed in Thread: TS3USB3200 Hi,
I am finding a low cost switch for the SATA signal. I have read the datasheet of ts3usb3200, this switch looks like to meet the demand. Because all of the parameters look like to meet the demand. The switch…
Part Number: TS3USB3000 Other Parts Discussed in Thread: TS3USB3200 , TMUX5412 Hi team,
Our customer is currently using the TS3USB3000RSER as a switch for USB 2.0 signal lines. However, this device has an active-low enable/control input.
Do you…
Part Number: TS3USB221 Other Parts Discussed in Thread: TS3USB3200 , TMUX1575 Hello
I'd like to know if TS3USB221 is suitable for separating I2S signal as below schematic?
Thank you!
Part Number: TL16C754B Other Parts Discussed in Thread: TS3USB3200 , TS5A23159 , TS5A3154 Hi there,
Is there any UART Mux in our portfolio? My customer is looking for a 1:2 mux.
TS3USB3200 seems OK but it's very high speed compared to UART.
Thank…