Other Parts Discussed in Thread: TS5A3166 Hi,Team,
My customer is using TS5A3166 to switch RS485 A/B bus.
The range of A/B bus is 0~5V. V+ is +5V. Datarate is 9600bps.
The IN pin is +5V. The analog input is +5V, the ouput is sitll with +1V level…
Other Parts Discussed in Thread: TS5A3166 , TS5A3167 Team: I have a question about the TS5A3166/TS5A3167 (SPST) analog switch device. Want to know if I can drive a current of about 125mA (instead of 100mA) through this device. Continuous switching current…
Part Number: TS5A3167 Other Parts Discussed in Thread: TS5A3166 , , TS5A4594 Tool/software: The banner title of the datasheet says this is a SPST BUT the Description says its a SPDT (DOUBLE throw, rather than SINGLE throw. The rest of the datasheet docuements…
Part Number: THVD2450V Other Parts Discussed in Thread: THVD2450 , TMUX1511 , TS5A3166 Tool/software: Hello,
I was planning to use the THVD2450V RS-485 transceiver because I want to drive the bus at 5V while powering the logic level signals from a 3…
Part Number: SN74LVC1G66 Other Parts Discussed in Thread: TS5A3166 Tool/software: Hello,
I have a question regarding the use of SN74LVC1G66 analog switch. We are looking to replace a onsemi part number NC7SZ66M5X that is going obsolete and the SN74LVC1G66…
Part Number: SN74CB3T1G125-Q1 Other Parts Discussed in Thread: TS5A3166-Q1 , SN3257-Q1 Tool/software: Hi Team,
Customer is looking for a Analog SW solution for 1ch RGMII signal SW between controller and GbE PHY.
Control SW on/off by GPIO 1.8V…
Part Number: TS5A1066 Other Parts Discussed in Thread: TS5A4624 , , TS5A3166 , TS5A3167 Hi team,
Does TS5A1066 support Isolation in Power-Down Mode as well as TS5A4624?
(i.e. Does COM or NO accept 3.3V when V+=0V?)
Best regards,
Itoh
Hi Ambroise,
We have connected a 25K ohm resistor between the TS5A3166 and GPIO pin of a microprocessor as a part of a low pass circuit. We wanted to make sure that the 25K ohm resistor has no effect on the input impedance of TS5A3166 . Ideally, if…
There is no device named "TS3A3166".
The automotive variant of the TS5A3166 is the TS5A3166-Q1. (It will not work with voltages outside its supply voltage, which might be a problem if your CAN bus has a common-mode voltage.)
Part Number: SN74CB3Q3306A Other Parts Discussed in Thread: TS5A3166 , , TS5A3167 I am designing a system with an RS485 bus. The bus is <1 m but long enough to require termination in both ends. At one end of the bus there is a main module that always…