Part Number: TSU6111 Other Parts Discussed in Thread: TS3USB221 Dear Team,
I sourced a part that can be a UART switch, could you help to confirm TSU6111 datasheet?
There are two output interfaces on TSU6111, one is USB and the other is UART, what…
Part Number: TSU6111 Other Parts Discussed in Thread: TSU6721 This is one of the most asked yet confusing where I need to charge the tablet and use the USB port as peripheral ( accessory ) simultaneously. I might disconnect the charger and then the tablet…
Part Number: TSU6111 Other Parts Discussed in Thread: BQ24392 Hi support team,
My customer is interested on TSU6111A. But they have a concern about the accessories detection. They want to know if the accessory is attached and don't care about what type…
Part Number: TSU6111 Dear e2e community,
When when my customer connects a usb cable, the ADC value indicates "11111". The switch seems to be in open state at that time.
As there are 4 possible Switch States, for this ADC value, which one should we…
Other Parts Discussed in Thread: TSU6111 Dear Support team,
Can RxD and TxD ports of TSU6111 support bidirectional I2C instead of UART?
Best regards,
Hiro Takahashi
Part Number: TSU6111 Could we set the TSU6111 to Factory Mode Cable - Boot On UART with resitstor that 619K when power on with hardware function for default mode design.
Hi Brian
I've just looked at the app note here. The part TSU6111 datasheet says:
"ESD Performance DP/DM/ID/VBUS to GND – ±8kV Contact Discharge (IEC 61000-4-2)
Surge Protection on VBUS/DP/DM – USB Connector Pins Without External Components"
But app…
Other Parts Discussed in Thread: TSU6111 Hello. I have a question about TSU6111's UART mode.
1. When its second downstream port (UART/HS USB) is in UART mode (bits 2-4 and bits 5-7 are "011"), this port acts as USB-to-Serial controller?
2. And when…